Skip to main content
sbg29
Associate II
April 16, 2020
Question

Issue to program MMC using STM32_Programmer_CLI tool

Hello,

I am facing an issue with flashing my MMC on STM32MP157C-DK2 board using STM32_Programmer_CLI (linux version)

I have created a flash layout file like this:

#opt	Id	Name	Type	Device	Offset	Binary
-	0x01	fsbl-boot	Binary	none	0x0	tf-a-loader.stm32
-	0x03	ssbl-boot	Binary	none	0x0	u-boot-loader-optee.stm32
P	0x04	fsbl1	Binary	mmc0	0x4400	tf-a.stm32
P	0x05	fsbl2	Binary	mmc0	0x00044400	tf-a.stm32
P	0x06	ssbl	Binary	mmc0	0x00084400	u-boot.stm32
P	0x07	teeh	Binary	mmc0	0x00184400	tee-header_v2.stm32
P	0x08	teed	Binary	mmc0	0x001C4400	tee-pageable_v2.stm32
P	0x09	teex	Binary	mmc0	0x00204400	tee-pager_v2.stm32
P	0x10	ssbl-env	Binary	mmc0	0x00244400	u-boot-env.bin
P	0x11	ssbl-env-red	Binary	mmc0	0x00246400	u-boot-env.bin
P	0x12	fit1	Binary	mmc0	0x00248400	fit_kernel_dtb.itb
P	0x13	rfs1	Binary	mmc0	0x00848400	rootfs.squashfs
P	0x14	fit2	Binary	mmc0	0x02048400	fit_kernel_dtb.itb
P	0x15	rfs2	Binary	mmc0	0x02648400	rootfs.squashfs

After loading tf-a and u-boot and starting U-Boot in RAM, U-Boot fails to load binaries for flashing them into MMC

If I use a tsv file (with RawImage of SDcard as defined bellow), there is no issue but I don't want to choose this option because of time issue. Downloading and burning a complete image of MMC takes more time than downloading and burning individually images.

Partitions size is bigger than images size.

#opt	Id	Name	Type	Device	Offset	Binary
-	0x01	fsbl-boot	Binary	none	0x0	tf-a-loader.stm32
-	0x03	ssbl-boot	Binary	none	0x0	u-boot-loader-optee.stm32
P	0x32	sdcard	RawImage	mmc0	0x0	sdcard.img

Here are the logs of STM32_Programmer_CLI:

USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 0035002E3338510B39303435
FW version : 0x0110
Device ID : 0x0500
Device name : STM32MPxxx
Device type : MPU
Device CPU : Cortex-A7
 
Start Embedded Flashing service
 
Memory Programming ...
Opening and parsing file: tf-a-loader.stm32
 File : tf-a-loader.stm32
 Size : 245384 Bytes
 Partition ID : 0x01 
 
Download in Progress:
[==================================================] 100% 
 
File download complete
Time elapsed during download operation: 00:00:03.103
 
RUNNING Program ... 
 PartID: :0x01 
Start operation done successfully at partition 0x01
 
Flashlayout Programming ...
[==================================================] 100% 
Running Flashlayout Partition ...
Flashlayout partition started successfully
 
 
Memory Programming ...
Opening and parsing file: u-boot-loader-optee.stm32
 File : u-boot-loader-optee.stm32
 Size : 810605 Bytes
 Partition ID : 0x03 
 
Download in Progress:
[==================================================] 100% 
 
File download complete
Time elapsed during download operation: 00:00:08.610
 
RUNNING Program ... 
 PartID: :0x03 
 
reconnecting the device ...
 
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x0000
SN : 0035002E3338510B39303435
FW version : 0x0110
Device ID : 0x0500
Start operation done successfully at partition 0x03
Error: an error occured while uploading data from the virtual partition 0xF1
Received PhaseID == 0xFF, system is going to reboot

Here are the U-Boot Logs:

U-Boot 2018.11-stm32mp-r4 (Nov 14 2018 - 16:10:06 +0000)
 
CPU: STM32MP157CAC Rev.B
Model: STMicroelectronics STM32MP157C-DK2 Discovery Board
Board: stm32mp1 in op-tee mode (st,stm32mp157c-dk2)
Board: MB1272 Var2 Rev.C-01
DRAM: 480 MiB
Clocks:
- MPU : 650 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
****************************************************
* WARNING 500mA power supply detected *
* Current too low, use a 3A power supply! *
****************************************************
 
NAND: 0 MiB
MMC: STM32 SDMMC2: 0, STM32 SDMMC2: 1
In: serial
Out: serial
Err: serial
Net: eth0: ethernet@5800a000
Hit any key to stop autoboot: 0 
Boot over usb0!
partitions : Writing GPT: success!
done
DFU alt info setting: done
crq->brequest:0x0
crq->brequest:0x0

I don't have any information in LOGs helping me to understand what is the problem.

Does anyone know what is wrong in the first tsv file ?

Best regards,

Sebastien

This topic has been closed for replies.

1 reply

Olivier GALLIEN
ST Technical Moderator
April 22, 2020

Hi @sbg29

As a first hint could you please manage to get a proper supply voltage.

Seems you are using a weak one

****************************************************

* WARNING 500mA power supply detected *

* Current too low, use a 3A power supply! *

****************************************************

We already have cases where this lead to erratic behavior during flash operation.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.