Skip to main content
Visitor II
April 10, 2025
Question

Interrupt priority configuration error in code generated by CubeMX for stm32mp135

An error in the interrupt priority configuration of the STM32MP135 code generated by CubeMX will result in all interrupts being set incorrectly. For example, if you set the interrupt priority for EXTI0 to 10 in CubeMX, the code will be generated:

IRQ_SetPtiority(EXTI0_IRQn, 10);


And the correct way is to shift the priority by 3 bits:

IRQ_SetPtiority(EXTI0_IRQn, 10<<3);

 

Can this be fixed in future releases?

This topic has been closed for replies.