Get ready for the STM32 Summit 2026 | Online, November 3
Ask questions and find answers on STM32 microprocessors software development tools.
Most recent activity
1 Select STM32MP151 (This case AAAx)2. Select an GPIOx and set to GIPIO_EXTx 3. Goto NVIC: EXTI option is disabled (Checkbox cannot be selected)4. Goto GPIO : Pin can be configured as interrupt How to enable interrupts for NVIC for GPIO's in order to generate the code ? See pictures. CubeMX 5.3.0, Linux
cube programmer doesn't work on linuxIt gives error JavaFX NOT installed => warn userbut javafx is installed (sudo apt-get install openjfx)Linux Mint 19.2 Tina4.15.0-60-generic #67-Ubuntu SMP
while selecting STM32MP157A in cubemx,it shows STM32cubemx CAN NOT LOAD THIS MCUdialog box.
Right now it appears we must use AC6. Will it be long before CubeIDE works?
Hi ST Community,i am trying to debug firmware on cortex-m4 of STM32MP157-Eval. i had success debugging OpenAmp_TTY_echo example as instructed in https://wiki.st.com/stm32mpu/wiki/Modify,_rebuild_and_reload_a_firmware. But while trying to debug a simple hello world example by same method, the Debug button is always deactive and i am not getting any kind of error or missing setting on debug window as well.Could you please guide me, what i am missing here?Best Regards,Bhinder
Hi ST Community,i am using STM32CubeIDE. But i can not create an example project as i am getting the following error. But according to old posts related to STM32MP157, other users have created the example project successfully. Need some help please for getting started.i am using STM32CubeIDE v1.0.0. Best Regards,Usman
Hello,my STM32MP1157C-DK2 is up and running. I can use the Stlink with other tools. However stm32cubeprogrammer does no show the disco stlink. Is this a know issue?
Hi, I use STM32CubeProgrammer to download file into dk2 board. I am confuse about the tsv file. Could you give more detail this file and programming steps description? How can i modify it to download files into my custom board. And I can not found the AN5275 file.Could you support it?
Hi, I'm trying to test the openAMP_TTY_echo from STM32Cube_FW_MP1_V1.0.1. It compiles ok. I try the installation from : https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157C-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-M4/Modify,_rebuild_and_reload_a_firmware#but I fail to get the info from the "debugger" in [Upload and start the firmware].It wants "OpenOCD Setup" but there is no info on the wiki about that. So it loads the firmware ok but then failed with gdb/OpenOCD... My openAMP_TTY.cfg is empty!ThanksAnthony Harivel
..
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.