Skip to main content
FHyat.1
Associate
June 8, 2022
Question

How to run the sample OpenAMP_TTY_echo program in STM32CubeIDE

I'm following a tutorial for setting up the STM32MP157C-DK2. I'm on the step for running the OpenAMP_TTY sample program. However, when I try to build the program, I get a whole bunch or errors as follows:

make -j8 all 
arm-none-eabi-gcc -o "OpenAMP_TTY_echo_CM4.elf" @"objects.list" -mcpu=cortex-m4 -T"/home/ben/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Developer-Package/STM32Cube_FW_MP1_V1.5.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo/STM32CubeIDE/CM4/STM32MP157CAAX_RAM.ld" --specs=nosys.specs -Wl,-Map="OpenAMP_TTY_echo_CM4.map" -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
/usr/lib/gcc/arm-none-eabi/9.2.1/../../../arm-none-eabi/bin/ld: ./Application/Startup/startup_stm32mp157caax.o: in function `LoopFillZerobss':
/home/ben/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Developer-Package/STM32Cube_FW_MP1_V1.5.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo/STM32CubeIDE/CM4/Application/Startup/startup_stm32mp157caax.s:90: undefined reference to `SystemInit'
/usr/lib/gcc/arm-none-eabi/9.2.1/../../../arm-none-eabi/bin/ld: ./Application/User/main.o: in function `main':
/home/ben/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Developer-Package/STM32Cube_FW_MP1_V1.5.0/Projects/STM32MP157C-DK2/Applications/OpenAMP
collect2: error: ld returned 1 exit status
make: *** [makefile:63: OpenAMP_TTY_echo_CM4.elf] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.

I abbreviated the error, but there are 82 of them that say "undefined reference to." I'm thinking that the issue might have something to do with setting the source of the SDK or perhaps with setting up the environment, but I'm not sure. Any help or guidance is greatly appreciated.

This topic has been closed for replies.

7 replies

FHyat.1
FHyat.1Author
Associate
June 8, 2022
Olivier GALLIEN
ST Technical Moderator
June 9, 2022

Hi @FHyat.1​ ,

Strange this is usually straigthforward.

Can you check and provide CubeIDE and Cube Package version you are using ?

Else, your log show an error on final step of the build. Could you rather provide very first error after a clean or complete log ?

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
FHyat.1
FHyat.1Author
Associate
June 9, 2022

CubeIDE information:

  • Version: 1.9.0
  • Build: 12015_20220302_0855 (UTC)

I also have the 1.8.0 version installed, as I was unsure if I wanted to use environment 3.0.0 or 3.1.0.

Here's the beginning section of the error that I'm getting:

make -j8 all 
arm-none-eabi-gcc -o "OpenAMP_TTY_echo_CM4.elf" @"objects.list" -mcpu=cortex-m4 -T"/home/ben/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Developer-Package/STM32Cube_FW_MP1_V1.5.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo/STM32CubeIDE/CM4/STM32MP157CAAX_RAM.ld" --specs=nosys.specs -Wl,-Map="OpenAMP_TTY_echo_CM4.map" -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
/usr/lib/gcc/arm-none-eabi/9.2.1/../../../arm-none-eabi/bin/ld: ./Application/Startup/startup_stm32mp157caax.o: in function `LoopFillZerobss':
/home/ben/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Developer-Package/STM32Cube_FW_MP1_V1.5.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo/STM32CubeIDE/CM4/Application/Startup/startup_stm32mp157caax.s:90: undefined reference to `SystemInit'
/usr/lib/gcc/arm-none-eabi/9.2.1/../../../arm-none-eabi/bin/ld: ./Application/User/main.o: in function `main':
/home/ben/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Developer-Package/STM32Cube_FW_MP1_V1.5.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo/Src/main.c:88: undefined reference to `HAL_Init'
/usr/lib/gcc/arm-none-eabi/9.2.1/../../../arm-none-eabi/bin/ld: /home/ben/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Developer-Package/STM32Cube_FW_MP1_V1.5.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo/Src/main.c:97: undefined reference to `HAL_GetTick'

Kevin HUBER
ST Employee
June 9, 2022

Hi @FHyat.1​,

The official version of CubeIde for ecosystem v3.1 is: 1.8.0

as explained in the ecosystem release note: https://wiki.st.com/stm32mpu/wiki/STM32MP15_ecosystem_release_note_-_v3.1.0#STM32CubeIDE

But, it should works with version 1.9.0 too. So for a test purpose, I made a try with the 1.9.0 and the project OpenAMP_TTY_echo, the build is functional.

By reading your traces, it looks like a problem during the importation of the project. Please can you send me a screenshot of your complete CubeIde window? I would like to especially see the project tree (on the left side).

One more thing, I can see in my build traces that by default, I am building with:

make -j3 all

and in your traces, we can see:

make -j8 all 

Which operating system are you using?

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Kevin HUBER
ST Employee
June 28, 2022

Hello @FHyat.1​ ,

Yes the -j8 is related to the number of cores used, you are right.

For information the ST solution is tested on Ubuntu 20.04 and 18.04, not on the other distribution.

The recommended setup is Ubuntu 20.04 LTS:

https://wiki.st.com/stm32mpu-ecosystem-v3/wiki/PC_prerequisites#Linux-C2-AE_PC

So this is maybe a problem due to Debian, but I do not think this is the case.

Your problem looks like the project is not able to find the drivers code of your STM32Cube_FW_MP1_V1.5.0.

For example in your traces:

undefined reference to `HAL_GetTick'

This function is normally defined in STM32Cube_FW_MP1_V1.5.0/Drivers/STM32MP1xx_HAL_Driver/Src/stm32mp1xx_hal.c at line 359.

So if your linker is not able to find it, this is because the file was not built during the build.

Please can you make a right click then properties on your project "OpenAMP_TTY_echo_CM4", like this:

0693W00000NsxkrQAB.png 

I would like to see the location of the tty_echo project that you included into cubeIde.

Then please

  • right click again of the project "OpenAMP_TTY_echo_CM4" and "clean Project".
  • build again the project
  • send here the complete build log. (not only the linker).

In your two previous message you only sent the linker traces, but not the one from the build.

Normally they must start we the file.c to build, looks like below:

make -j3 all 
arm-none-eabi-gcc "/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/STM32Cube_FW_MP1_V1.5.0/Middlewares/Third_Party/OpenAMP/virtual_driver/virt_uart.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DMETAL_MAX_DEVICE_REGIONS=2 -DUSE_HAL_DRIVER -DSTM32MP157Cxx -D__LOG_TRACE_IO_ -DCORE_CM4 -DDEBUG -DNO_ATOMIC_64_SUPPORT -DMETAL_INTERNAL -DVIRTIO_SLAVE_ONLY -c -I../../../../../../../../Drivers/STM32MP1xx_HAL_Driver/Inc -I../../../../../../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32MP1xx/Include -I../../../../../../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../../../../../../Drivers/STM32MP1xx_HAL_Driver/Inc/Legacy -I../../../../../../../../Drivers/BSP/STM32MP15xx_DISCO -I../../../Inc -I../../../../../../../../Drivers/CMSIS/Include -I../../../../../../../../Middlewares/Third_Party/OpenAMP/virtual_driver -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Middlewares/OpenAMP/virtual_driver/virt_uart.d" -MT"Middlewares/OpenAMP/virtual_driver/virt_uart.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Middlewares/OpenAMP/virtual_driver/virt_uart.o"
arm-none-eabi-gcc "/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/STM32Cube_FW_MP1_V1.5.0/Middlewares/Third_Party/OpenAMP/open-amp/lib/virtio/virtio.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DMETAL_MAX_DEVICE_REGIONS=2 -DUSE_HAL_DRIVER -DSTM32MP157Cxx -D__LOG_TRACE_IO_ -DCORE_CM4 -DDEBUG -DNO_ATOMIC_64_SUPPORT -DMETAL_INTERNAL -DVIRTIO_SLAVE_ONLY -c -I../../../../../../../../Drivers/STM32MP1xx_HAL_Driver/Inc -I../../../../../../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32MP1xx/Include -I../../../../../../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../../../../../../Drivers/STM32MP1xx_HAL_Driver/Inc/Legacy -I../../../../../../../../Drivers/BSP/STM32MP15xx_DISCO -I../../../Inc -I../../../../../../../../Drivers/CMSIS/Include -I../../../../../../../../Middlewares/Third_Party/OpenAMP/virtual_driver -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Middlewares/OpenAMP/open-amp/virtio/virtio.d" -MT"Middlewares/OpenAMP/open-amp/virtio/virtio.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Middlewares/OpenAMP/open-amp/virtio/virtio.o"

It will help me to understand the error that you encounter.

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.