Skip to main content
bdill.1
Associate II
May 31, 2023
Question

How do I invoke the Yocto build to create a system image with the STM32CubeIDE? I haven't found documentation on how to actually use the tools to generate the image that can be "burned" to a microSD that the STM32MP157D-DK1 board can boot.

..

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
May 31, 2023

Hi @bdill.1​ ,

maybe those links could help you:

https://wiki.st.com/stm32mpu/wiki/How_to_install_the_Yocto_Project_SDK_in_STM32CubeIDE

https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package#Building_the_OpenSTLinux_distribution

https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Let%27s_start/Populate_the_target_and_boot_the_image

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent