Skip to main content
msj
Associate
February 28, 2023
Question

How can you use CubeProgrammer_API.dll to do Secure Firmware Install and SSP?

There are a number of functions used by the STM32_Programmer_CLI to accomplish secure firmware install and secure secrets provisioning (STM32U5 and STM32MP13 being the targets). I'm looking at what's needed to integrate this process into build/program/test harness - ideally via the API.

 

None of the examples seem to describe how to accomplish this via API. I was able to retrieve the chip certificate for the U5 via the API after wiretapping/verbose debugging of the CLI tool. It pretty straight forwardly reads a specific address via the DFU. What I couldn't figure out is where this address is coming from. On another board (L5) its a different address. I'd really like a general solution for this.

 

Is there documentation or examples of using the API to accomplish the tasks described in AN4992 (STM32MCUs secure firmware install (SFI) overview) or AN5510 (Overview of the secure secret provisioning (SSP) on STM32MP1 Series)?

 

 

This topic has been closed for replies.

3 replies

OlivierK
ST Technical Moderator
March 9, 2023

Hi msj (Community Member)

There will be an API example for SSP provided In the next revision of CubeProgrammer v2.14.0. For SFI there is some demand to have the same but it is not yet forecasted.

Rgds,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
msj
msjAuthor
Associate
March 17, 2023

Thanks! Could you tell me approximately when that will be released?

OlivierK
ST Technical Moderator
May 25, 2023

Hi msj (Community Member)

The release forecast for 2.14 is for end of June.

Rgds,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.