Skip to main content
Associate II
May 27, 2025
Solved

Fail the image flashing on STM32MP257F-EV1

Dear ST Developer Support,

I download the STM32MP2 android 13 images from https://www.st.com/en/embedded-software/stm32mp2droidsta.html#get-software .

When I flash the st-android-13.0.0-2024-07-31-stm32mp257f-ev1-emmc-starter images by using STM32CubeProgrammer v2.19 for windows, I would fail on flashing super.img phase.

The error message show "Error while reading the file".

Would you help me solve this problem. Thanks.

 

I attached the fail logs

11:40:58 : STM32CubeProgrammer API v2.19.0 | Windows-64Bits
11:41:07 : UR connection mode is defined with the HWrst reset mode
11:41:07 : USB speed : High Speed (480MBit/s)
11:41:07 : Manuf. ID : STMicroelectronics
11:41:07 : Product ID : DFU in HS Mode @Device ID /0x505, @Revision ID /0x2000
11:41:07 : SN : 002F00414136500B00373653
11:41:07 : DFU protocol: 1.1
11:41:07 : Board : --
11:41:07 : Device ID : 0x0505
11:41:11 : Read TSV File: D:\Project\STM\STM32MP257F\Android-13\en.st-android-13.0.0-2024-07-31-stm32mp257f-ev1-emmc-starter\st-android-13.0.0-2024-07-31-stm32mp257f-ev1-emmc-starter\FlashLayout_emmc_optee.tsv
11:41:11 : Number of partitions: 20
11:41:13 : Start Embedded Flashing service
11:41:13 : Opening and parsing file: fsbl-programmer.img
11:41:13 : Memory Programming ...
11:41:13 : File : fsbl-programmer.img
11:41:13 : Size : 182.86 KB
11:41:13 : Partition ID : 0x01
11:41:13 : Download in Progress:
11:41:14 : File download complete
11:41:14 : Time elapsed during download operation: 00:00:01.560
11:41:14 : RUNNING Program ...
11:41:14 : PartID: :0x01
11:41:15 : Reconnecting the device ...
11:41:15 : USB speed : High Speed (480MBit/s)
11:41:15 : Manuf. ID : STMicroelectronics
11:41:15 : Product ID : DFU @Device ID /0x505, @Revision ID /0x0011, @Name /STM32MP257FAI Rev.Y,
11:41:15 : SN : 002F00414136500B00373653
11:41:15 : DFU protocol: 1.1
11:41:15 : Board : --
11:41:15 : Device ID : 0x0505
11:41:15 : Device name : STM32MP257FAI Rev.Y
11:41:15 : Device type :
11:41:15 : Device CPU :
11:41:15 : Start operation done successfully at partition 0x01
11:41:15 : Opening and parsing file: fip-ddr-programmer.img
11:41:15 : Memory Programming ...
11:41:15 : File : fip-ddr-programmer.img
11:41:15 : Size : 28.79 KB
11:41:15 : Partition ID : 0x02
11:41:15 : Download in Progress:
11:41:15 : File download complete
11:41:15 : Time elapsed during download operation: 00:00:00.026
11:41:15 : RUNNING Program ...
11:41:15 : PartID: :0x02
11:41:16 : Reconnecting the device ...
11:41:16 : USB speed : High Speed (480MBit/s)
11:41:16 : Manuf. ID : STMicroelectronics
11:41:16 : Product ID : DFU @Device ID /0x505, @Revision ID /0x0011, @Name /STM32MP257FAI Rev.Y,
11:41:16 : SN : 002F00414136500B00373653
11:41:16 : DFU protocol: 1.1
11:41:16 : Board : --
11:41:16 : Device ID : 0x0505
11:41:16 : Device name : STM32MP257FAI Rev.Y
11:41:16 : Device type :
11:41:16 : Device CPU :
11:41:16 : Start operation done successfully at partition 0x02
11:41:16 : Opening and parsing file: fip.img
11:41:16 : Memory Programming ...
11:41:16 : File : fip.img
11:41:16 : Size : 2.64 MB
11:41:16 : Partition ID : 0x03
11:41:16 : Download in Progress:
11:41:18 : File download complete
11:41:18 : Time elapsed during download operation: 00:00:02.187
11:41:18 : RUNNING Program ...
11:41:18 : PartID: :0x03
11:41:18 : Reconnecting the device ...
11:41:24 : USB speed : High Speed (480MBit/s)
11:41:24 : Manuf. ID : STMicroelectronics
11:41:24 : Product ID : USB download gadget@Device ID /0x505, @Revision ID /0x0011, @Name /STM32MP257FAI Rev.Y,
11:41:24 : SN : 002F00414136500B00373653
11:41:24 : DFU protocol: 1.1
11:41:24 : Board : --
11:41:24 : Device ID : 0x0505
11:41:24 : Device name : STM32MP257FAI Rev.Y
11:41:24 : Device type :
11:41:24 : Device CPU :
11:41:24 : Start operation done successfully at partition 0x03
11:41:24 : Flashlayout Programming ...
11:41:24 : Running Flashlayout Partition ...
11:41:25 : Reconnecting the device ...
11:41:25 : USB speed : High Speed (480MBit/s)
11:41:25 : Manuf. ID : STMicroelectronics
11:41:25 : Product ID : USB download gadget@Device ID /0x505, @Revision ID /0x0011, @Name /STM32MP257FAI Rev.Y,
11:41:25 : SN : 002F00414136500B00373653
11:41:25 : DFU protocol: 1.1
11:41:25 : Board : --
11:41:25 : Device ID : 0x0505
11:41:25 : Device name : STM32MP257FAI Rev.Y
11:41:25 : Device type :
11:41:25 : Device CPU :
11:41:25 : Flashlayout partition started successfully
11:41:25 : Opening and parsing file: fsbl-optee.img
11:41:25 : Memory Programming ...
11:41:25 : File : fsbl-optee.img
11:41:25 : Size : 198.90 KB
11:41:25 : Partition ID : 0x04
11:41:25 : Download in Progress:
11:41:25 : File download complete
11:41:25 : Time elapsed during download operation: 00:00:00.055
11:41:25 : RUNNING Program ...
11:41:25 : PartID: :0x04
11:41:25 : Start operation done successfully at partition 0x04
11:41:25 : Opening and parsing file: fsbl-optee.img
11:41:25 : Memory Programming ...
11:41:25 : File : fsbl-optee.img
11:41:25 : Size : 198.90 KB
11:41:25 : Partition ID : 0x05
11:41:25 : Download in Progress:
11:41:25 : File download complete
11:41:25 : Time elapsed during download operation: 00:00:00.060
11:41:25 : RUNNING Program ...
11:41:25 : PartID: :0x05
11:41:25 : Start operation done successfully at partition 0x05
11:41:25 : Opening and parsing file: fip.img
11:41:25 : Memory Programming ...
11:41:25 : File : fip.img
11:41:25 : Size : 2.64 MB
11:41:25 : Partition ID : 0x06
11:41:25 : Download in Progress:
11:41:26 : File download complete
11:41:26 : Time elapsed during download operation: 00:00:00.693
11:41:26 : RUNNING Program ...
11:41:26 : PartID: :0x06
11:41:26 : Start operation done successfully at partition 0x06
11:41:26 : Opening and parsing file: splash.img
11:41:26 : Memory Programming ...
11:41:26 : File : splash.img
11:41:26 : Size : 166.05 KB
11:41:26 : Partition ID : 0x10
11:41:26 : Download in Progress:
11:41:26 : File download complete
11:41:26 : Time elapsed during download operation: 00:00:00.048
11:41:26 : RUNNING Program ...
11:41:26 : PartID: :0x10
11:41:26 : Start operation done successfully at partition 0x10
11:41:26 : Opening and parsing file: vbmeta.img
11:41:26 : Memory Programming ...
11:41:26 : File : vbmeta.img
11:41:26 : Size : 8.00 KB
11:41:26 : Partition ID : 0x11
11:41:26 : Download in Progress:
11:41:26 : File download complete
11:41:26 : Time elapsed during download operation: 00:00:00.007
11:41:26 : RUNNING Program ...
11:41:26 : PartID: :0x11
11:41:26 : Start operation done successfully at partition 0x11
11:41:26 : Opening and parsing file: vbmeta.img
11:41:26 : Memory Programming ...
11:41:26 : File : vbmeta.img
11:41:26 : Size : 8.00 KB
11:41:26 : Partition ID : 0x12
11:41:26 : Download in Progress:
11:41:26 : File download complete
11:41:26 : Time elapsed during download operation: 00:00:00.013
11:41:26 : RUNNING Program ...
11:41:26 : PartID: :0x12
11:41:26 : Start operation done successfully at partition 0x12
11:41:26 : Opening and parsing file: boot.img
11:41:26 : Memory Programming ...
11:41:26 : File : boot.img
11:41:26 : Size : 64.00 MB
11:41:26 : Partition ID : 0x21
11:41:26 : Download in Progress:
11:41:47 : File download complete
11:41:47 : Time elapsed during download operation: 00:00:20.862
11:41:47 : RUNNING Program ...
11:41:47 : PartID: :0x21
11:41:47 : Start operation done successfully at partition 0x21
11:41:47 : Opening and parsing file: boot.img
11:41:47 : Memory Programming ...
11:41:47 : File : boot.img
11:41:47 : Size : 64.00 MB
11:41:47 : Partition ID : 0x22
11:41:47 : Download in Progress:
11:42:08 : File download complete
11:42:08 : Time elapsed during download operation: 00:00:21.023
11:42:08 : RUNNING Program ...
11:42:08 : PartID: :0x22
11:42:08 : Start operation done successfully at partition 0x22
11:42:08 : Opening and parsing file: vendor_boot.img
11:42:08 : Memory Programming ...
11:42:08 : File : vendor_boot.img
11:42:08 : Size : 16.00 MB
11:42:08 : Partition ID : 0x23
11:42:08 : Download in Progress:
11:42:14 : File download complete
11:42:14 : Time elapsed during download operation: 00:00:05.298
11:42:14 : RUNNING Program ...
11:42:14 : PartID: :0x23
11:42:14 : Start operation done successfully at partition 0x23
11:42:14 : Opening and parsing file: vendor_boot.img
11:42:14 : Memory Programming ...
11:42:14 : File : vendor_boot.img
11:42:14 : Size : 16.00 MB
11:42:14 : Partition ID : 0x24
11:42:14 : Download in Progress:
11:42:19 : File download complete
11:42:19 : Time elapsed during download operation: 00:00:05.229
11:42:19 : RUNNING Program ...
11:42:19 : PartID: :0x24
11:42:19 : Start operation done successfully at partition 0x24
11:42:19 : Opening and parsing file: dtbo.img
11:42:19 : Memory Programming ...
11:42:19 : File : dtbo.img
11:42:19 : Size : 512.00 KB
11:42:19 : Partition ID : 0x25
11:42:19 : Download in Progress:
11:42:19 : File download complete
11:42:19 : Time elapsed during download operation: 00:00:00.135
11:42:19 : RUNNING Program ...
11:42:19 : PartID: :0x25
11:42:19 : Start operation done successfully at partition 0x25
11:42:19 : Opening and parsing file: dtbo.img
11:42:19 : Memory Programming ...
11:42:19 : File : dtbo.img
11:42:19 : Size : 512.00 KB
11:42:19 : Partition ID : 0x26
11:42:19 : Download in Progress:
11:42:19 : File download complete
11:42:19 : Time elapsed during download operation: 00:00:00.134
11:42:19 : RUNNING Program ...
11:42:19 : PartID: :0x26
11:42:19 : Start operation done successfully at partition 0x26
11:42:19 : Opening and parsing file: misc.img
11:42:19 : Memory Programming ...
11:42:19 : File : misc.img
11:42:19 : Size : 2.03 KB
11:42:19 : Partition ID : 0x27
11:42:19 : Download in Progress:
11:42:19 : File download complete
11:42:19 : Time elapsed during download operation: 00:00:00.006
11:42:19 : RUNNING Program ...
11:42:19 : PartID: :0x27
11:42:19 : Start operation done successfully at partition 0x27
11:42:19 : Opening and parsing file: super.img
11:42:19 : Memory Programming ...
11:42:19 : File : super.img
11:42:19 : Size : 1.37 GB
11:42:19 : Partition ID : 0x28
11:42:19 : Download in Progress:
11:49:57 : Error: Error while reading the file

 

 

This topic has been closed for replies.
Tim_hoBest answer
Associate II
June 24, 2025

Solution:

I try to use the older CubeProgrammer version v2.17 or v2.18, the problem could be solved. The super.img could flash successfully. I think the root cause is CubeProgrammer version problem.

6 replies

Senior III
May 27, 2025

Check if super.img is Corrupted or Incomplete

Go to the directory:

D:\Project\STM\STM32MP257F\Android-13\en.st-android-13.0.0-2024-07-31-stm32mp257f-ev1-emmc-starter\st-android-13.0.0-2024-07-31-stm32mp257f-ev1-emmc-starter\

 

Try to open super.img using a hex editor or simply right-click → Properties → check the file size. Compare the size with the official one (should be several GB).

If it’s too small (e.g. a few KB), the archive may have failed to extract properly, or the download was corrupted.

 

Tim_hoAuthor
Associate II
May 27, 2025

Dear ST Developer Support,

I have checked the super.img size, it is about 1.36GB.

I attach the properties screenshot file.

Do you have any idea? Thanks.

Associate II
June 13, 2025
Hi @Tim_ho,
     I used CubeProgrammer to flash images, and I also meet error problem when I flash super.img.It reports that "Error: Error while reading the file" the same to your error.
I try to use stm32cubeprg-win64-v2-17 to flash the same image today, and it doesn't have the error when it flash super.img now. You can try to use stm32cubeprg-win64-v2-17 to flash image.
Tim_hoAuthorBest answer
Associate II
June 24, 2025

Solution:

I try to use the older CubeProgrammer version v2.17 or v2.18, the problem could be solved. The super.img could flash successfully. I think the root cause is CubeProgrammer version problem.

Aziz BRIGUI
ST Technical Moderator
June 24, 2025

Hello all,

This is a known issue in CubeProgrammer v2.19 and is reported internally (Case n°208176).

Issue will be fixed in the next release coming beginning of next month.

Aziz 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.