Skip to main content
Associate III
Aug 12, 2025 8:07 AM UTC
Solved

Enable analyzers on the CubeIDE

Hi there,

I'm working on a STM32MP135 project.

I'd like to see some information on the Build Analyzer and/or Static stack analyzer but they always report the grids empty.

The project is compiled with the -fstack-usage and debualt Debug level (-g).

I checked that for each source files of the project are generated the .cyclo, .su, .d and .o files in the Debug directory.

The analyzers windows do not have a button to associate the project: but it seems not to be a problem with the latest relases.

So, why I cannot browse the analyzers data?

 

Version: 1.19.0

Build: 25607_20250703_0907 (UTC)

 

Thanks, regards

This topic has been closed for replies.
Souhaib MAZHOUDBest answer
ST Technical Moderator
Aug 13, 2025 10:36 AM UTC

Hello @SteMMo 

It seems that this is the same issue being discussed here.

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

SteMMoAuthor
Associate III
Aug 12, 2025 1:44 PM UTC

I've found that 'sometimes' works the 'Refresh' button .. sometimes .. the binaries are always rebuilt.

 

Souhaib MAZHOUDBest answer
ST Technical Moderator
Aug 13, 2025 10:36 AM UTC

Hello @SteMMo 

It seems that this is the same issue being discussed here.

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.