Skip to main content
iTTy
Associate III
January 23, 2026
Question

EGit Plugin Installation Error on STM32CubeIDE

Hi everyone,
I'm trying to install the EGit plug‑in on STM32CubeIDE version 1.14.1, but I'm running into persistent issues.
During the installation, the dependency calculation phase fails, and CubeIDE proposes alternative solutions. If I continue using the option to keep the original installation and modify only the required components, the process eventually ends with an installation error.
The exact same problem also occurs on STM32CubeIDE version 2.0.0, so it doesn’t seem related to a single release.
Below is the full error log I receive:

An error occurred while collecting items to be installed
session context was:(profile=STM32CubeIDE,
phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
No repository found containing: osgi.bundle,javax.annotation,1.3.5.v20230504-0748
No repository found containing: osgi.bundle,org.eclipse.emf.common,2.29.0.v20230916-0637
No repository found containing: osgi.bundle,org.eclipse.emf.ecore.xmi,2.36.0.v20231002-1156
No repository found containing: osgi.bundle,org.eclipse.jdt.core.compiler.batch,3.39.0.v20240820-0604
No repository found containing: osgi.bundle,com.jcraft.jsch,0.1.55.v20190404-1902
No repository found containing: osgi.bundle,com.jcraft.jzlib,1.1.1.v201205102305
No repository found containing: osgi.bundle,javaewah,1.1.6.v20160919-1400
No repository found containing: osgi.bundle,net.i2p.crypto.eddsa,0.3.0.v20181102-1323
No repository found containing: osgi.bundle,org.apache.commons.compress,1.18.0.v20181121-2221
No repository found containing: osgi.bundle,org.apache.log4j,1.2.15.v201012070815
No repository found containing: osgi.bundle,org.apache.sshd.osgi,2.2.0.v20190425-2127
No repository found containing: osgi.bundle,org.apache.sshd.sftp,2.2.0.v20190425-2127
No repository found containing: osgi.bundle,org.bouncycastle.bcpg,1.61.0.v20190602-1335
No repository found containing: osgi.bundle,org.bouncycastle.bcpkix,1.61.0.v20190602-1335
No repository found containing: osgi.bundle,org.bouncycastle.bcprov,1.61.0.v20190602-1335
No repository found containing: osgi.bundle,org.eclipse.egit,5.5.0.201909110433-r
No repository found containing: osgi.bundle,org.eclipse.egit.core,5.5.0.201909110433-r
No repository found containing: osgi.bundle,org.eclipse.egit.doc,5.5.0.201909110433-r
No repository found containing: org.eclipse.update.feature,org.eclipse.egit,5.5.0.201909110433-r
No repository found containing: osgi.bundle,org.eclipse.egit.ui,5.5.0.201909110433-r
No repository found containing: org.eclipse.update.feature,org.eclipse.emf.common,2.30.0.v20230916-0637
No repository found containing: org.eclipse.update.feature,org.eclipse.emf.ecore,2.36.0.v20231002-1156
No repository found containing: osgi.bundle,org.eclipse.jgit,5.5.0.201909110433-r
No repository found containing: osgi.bundle,org.eclipse.jgit.archive,5.5.0.201909110433-r
No repository found containing: org.eclipse.update.feature,org.eclipse.jgit,5.5.0.201909110433-r
No repository found containing: osgi.bundle,org.eclipse.jgit.ssh.apache,5.5.0.201909110433-r
No repository found containing: org.eclipse.update.feature,org.eclipse.jgit.ssh.apache,5.5.0.201909110433-r
No repository found containing: osgi.bundle,org.slf4j.api,1.7.2.v20121108-1250
No repository found containing: osgi.bundle,org.slf4j.impl.log4j12,1.7.2.v20131105-2200

Has anyone encountered this issue before or found a way to successfully install EGit on these CubeIDE versions? Any suggestions or workarounds would be greatly appreciated.
Thanks in advance!

iTTy

2 replies

DmitryR
Associate III
May 11, 2026

For me it has worked until version 2.0. Now the problem (on an update attempt) is, that the Eclipse Marketplace send a wrong answer. So it really seems to be a marketplace problem. But the Eclipse Foundation has a very inobvious structure and I have no idea where should I file this bug. ST is obviously also thinkung that it is not their problem. As far as an old version of the Egit works for me I could wait for a while, maybe the next update of the Eclipse or the Egit will solve the problem.

 

Regards,

Dmitry 

Associate
May 18, 2026

Hello

I think it can be incompatibility problem between stm32cubeide version and Egit version. I am using stm32cube 1.18.1, in market place the latest version of egit is only available for installation. The solution was to dowload the zip file of Egit version 7.0.0 and add install it using install new software section in help
This the link of version 7.0.0: https://www.eclipse.org/downloads/download.php?file=/egit/updates-7.0/org.eclipse.egit.repository-7.0.0.202409031743-r.zip