Skip to main content
Associate
July 6, 2026
Solved

Debugging Cortex-M33 application started by Linux remoteproc on STM32MP257

Hi ST team,

I am working with an STM32MP257 where Linux runs on the Cortex-A35 and a FreeRTOS application runs on the Cortex-M33. The M33 firmware is loaded and started by Linux using remoteproc.

The application is running correctly, but I would like to understand the recommended workflow for debugging the M33 application.

I have read the "Debug support" section of RM0457 and understand that the M33 can be accessed through the shared SWD/JTAG interface by selecting the appropriate Access Port. However, I'm still not clear on the recommended debug workflow when the M33 is managed by remoteproc.

My questions are:

  • Can STM32CubeIDE/ST-LINK attach to an already running M33 started by remoteproc, or should the M33 be stopped first?
  • If Linux has already loaded the firmware, should the debugger load only the ELF symbols instead of downloading the application again?
  • Is there any special OpenOCD/ST-LINK or CubeIDE configuration required for this use case?
  • Is there an ST application note or example demonstrating the recommended workflow?

My goal is to debug the M33 application with breakpoints, single-stepping, and variable inspection, similar to debugging a standalone STM32 MCU, while Linux continues to run on the A35.

Any guidance would be appreciated.

Thank you.

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
July 9, 2026

Hi ​@Hs26,

I guess you can start by looking at Develop on Arm® Cortex®-M33 - stm32mpu it will drive you to initial step setting up debug on CM33

Hope it help 

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

2 replies

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
July 9, 2026

Hi ​@Hs26,

I guess you can start by looking at Develop on Arm® Cortex®-M33 - stm32mpu it will drive you to initial step setting up debug on CM33

Hope it help 

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Hs26Author
Associate
July 29, 2026

Hi ​@Olivier GALLIEN ,

Thank you for the response! Actually, I did try that earlier and I was able to do following 

  • Pausing / Resuming Code via user buttons
  • Watching Expression / Live expression, SFRs etc..
  • Break Point Facility is not working  (which was my main objective for this post!)

Here is my console log when I start debug session

Open On-Chip Debugger 0.12.0+dev-00635-gddb0d32b4 (2025-11-07-10:06) [https://github.com/STMicroelectronics/OpenOCD]
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V3J16M9B5S1 (API v3) VID:PID 0483:3753
Info : Target voltage: 3.287060
Info : Unable to match requested speed 5000 kHz, using 3300 kHz
Info : Unable to match requested speed 5000 kHz, using 3300 kHz
Info : clock speed 3300 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : [STM32MP257FAIx.ap0] Examination succeed
Info : [STM32MP257FAIx.m33] Cortex-M33 r1p0 processor detected
Info : [STM32MP257FAIx.m33] target has 8 breakpoints, 4 watchpoints
Info : [STM32MP257FAIx.axi] Examination succeed
Info : gdb port disabled
Info : starting gdb server for STM32MP257FAIx.axi on 3334
Info : Listening on port 3334 for gdb connections
Info : gdb port disabled
Info : gdb port disabled
Info : gdb port disabled
Info : gdb port disabled
Info : starting gdb server for STM32MP257FAIx.m33 on 3333
Info : Listening on port 3333 for gdb connections
Info : gdb port disabled
Info : accepting 'gdb' connection on tcp/3333
[STM32MP257FAIx.m33] halted due to debug-request, current mode: Thread
xPSR: 0x89000000 pc: 0x80101ab8 msp: 0x80dfffc0
Info : New GDB Connection: 1, Target STM32MP257FAIx.m33, state: halted
Info : accepting 'gdb' connection on tcp/3333
Info : New GDB Connection: 2, Target STM32MP257FAIx.m33, state: halted
Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1799 ms). Workaround: increase "set remotetimeout" in GDB
Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1889 ms). Workaround: increase "set remotetimeout" in GDB
Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1221 ms). Workaround: increase "set remotetimeout" in GDB
Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1007 ms). Workaround: increase "set remotetimeout" in GDB
Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1197 ms). Workaround: increase "set remotetimeout" in GDB

Am I missing something? or doing something wrong?