Skip to main content
roland van straten
Associate III
November 15, 2024
Question

DDR Tuning MP157(f)

This post can be removed as I found out what was wrong...

But otherwise when you want to do DDR tuning some experienced quirks:

- RTFM twice!
- Make sure the target board is in Engineering Boot Mode!!
- Notices that latest CubeMX and STM32CubeProgrammer (2.17) does not find the path to the .._CLI even after setting it in CubeMX. Using an older version (2.16) did work.

- Besides the wiki, it is necessary to check the community too just to make sure you have the latest info. In the wiki there was mention of the U-Boot SPL to use. Then moment later the community post revealed that it was depreciated. So I got a copy of the DDRFW package from GitHub.

- The DDRFW package could generate a problem when building the software. I traced it back to a python script used as post build command. Installing `python-is-python3` solved that problem.

 

I managed to get the firmware running using STM32CubeIDE and debug mode. The use of the binary with CubeMX and CubeProgr (Tools/DDR Test Suite) needs to be tested again. At least using CubeIDE worked and I could see the DDR> prompt and do some testing.

 

> Wiki is sometimes missing articles that are under construction. Please update.

> It would be nice to bundle the Q&A that is only relevant for the latest release or label the posts as being for which release.

 

This topic has been closed for replies.