Skip to main content
Associate
October 17, 2023
Question

connection proxy error and no STM32 In DFU mode connected

hi guys i am trying to use  STM32MP135x-DK board with STM32CubeProgammer but after opening the software i got no internet connection  due to proxy setting and also no the program does not see any dfu device connected through usb .. can anyone help with this ? 

 

This topic has been closed for replies.

2 replies

amr5Author
Associate
October 17, 2023

i forgot to mention that i am using ubuntu 22.04

PatrickF
ST Employee
October 17, 2023

Hi @amr5 

1) proxy message is likely because you have access to internet thru a proxy. Please check CubeProgrammer documentation to setup a proxy (there is a menu in 'Help -> Proxy settings)

2) no DFU is not normal.

- Did you connect the right USB to the board (it is not the STLINK one) ?

- Did the board in DFU mode (check BOOT pins)

 

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent