Skip to main content
SKim.1761
Associate II
Oct 21, 2024 6:51 AM UTC
Question

wlan0 return brcmf_run_escan: error(-52)

Hello I got succeed wlan0 connect to my phone just yesterday

Ping 8.8.8.8 was worked and etc ok(without booting make 1m30s timeout)

But today it is not working at all with just doing same before

After enable and start wireless config with

 

systemctl enable wpa_supplicant@wlan0.service

 systemctl restart systemd-networkd.service

systemctl restart wpa_supplicant@wlan0.service

Or wpa_supplicant -B -iwlan0 -c /etc/wpa_supplicant/wpa_supplicant.conf

The error log is repeating on my console...

 

What should i check? 

 

Thanks

 

This topic has been closed for replies.

2 replies

PatrickF
ST Employee
Oct 21, 2024 12:49 PM UTC

Hi @SKim.1761 

please share more background on the issue

which board are you using ?

    STM32MP157F-DK2 ? else ?

Which OpenSTLinux ecosystem are you using ?

    Latest is v5.1.0: https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ecosystem_release_note

Maybe share full console log.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
SKim.1761
SKim.1761Author
Associate II
Nov 13, 2024 5:18 AM UTC

I am trying stm32mp157f-dk2 

I cannot answer about echosystem well,, just I can say just I am using starter package image

Anyway that problem is on smartphone's hotspot wifi only

I tried in home's wifi router it worked