Skip to main content
Lead
Jun 8, 2025 11:03 AM UTC
Question

Will DSI -> HDMI show the boot screen at startup?

The DSI can be transformed to HDMI using the ADV7535BCBZ chip. 

My question is: Will I be able to see the boot screen at startup directly when the HDMI is plugged in and Linux is booting? Or must Linux start the DSI later after the booting process?

This is for the STM32MP257FAK. 

This topic has been closed for replies.

1 reply

PPAGE.13
ST Employee
Jun 18, 2025 9:43 AM UTC

Hi,

if HDMI is plugged at startup, there will be no "ST" splash screen during uboot.

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.