Skip to main content
SChen.11
Associate III
August 2, 2019
Question

why the system workbench use stklink?

Hi, I use system workbench to debug example project. The serial port and ethernet over usb are recognized by system workbench. Now, the debuger step is using openocd to connect target board. I follow the below link to setting the debug configuration options.

https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157C-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-M4/Modify,_rebuild_and_reload_a_firmware

​

0690X0000097zpKQAQ.png

​

This topic has been closed for replies.

4 replies

Bumsik Kim
Senior
August 4, 2019

0690X000009813hQAA.pngIt uses OpenOCD (STLink) by default. Did you correctly set "thru Linux Core" in Startup tab, shown in the picture?

SChen.11
SChen.11Author
Associate III
August 4, 2019

I had select the production mode on startup tab window.Below is the screenshot.

0690X000009814QQAQ.png

SChen.11
SChen.11Author
Associate III
August 4, 2019

I use reinstall ubuntu 14.04 64bit to test it. It's also failed and got another error.

0690X0000098170QAA.png