Skip to main content
GRatt.1
Visitor II
June 8, 2020
Question

Which is the best way to shutdown/asleep and start/wake up STLinux through the M4 MCU ?

I am searching for the simplest way to do that, I think you ST engineers made this chip for this purpose so maybe there are intended ways to that

Thanks in advance

This topic has been closed for replies.

1 reply

Olivier GALLIEN
ST Technical Moderator
June 9, 2020

Hi @GRatt.1​ 

Please refer to all documentation related to Low Power management on MP1 :

Wiki : https://wiki.st.com/stm32mpu/wiki/Power_overview

AN5109 : https://www.st.com/resource/en/application_note/dm00449434-stm32mp1-series-using-lowpower-modes-stmicroelectronics.pdf

Then you can find a sample project in CubeFirmware Package under Projects\STM32MP157C-DK2\Applications\OpenAMP\OpenAMP_TTY_echo_wakeup

See scenario number 2 :  System Run Mode with CA7 in CStop and CM4 in CRun

Which looks to be the one you are interested in. ( A7 wakeup from M4)

Note that shutdown/restart A7 while M4 is running is not supported.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.