Skip to main content
Gencay
Associate III
September 7, 2022
Question

What should I do If I use a LVDS screen instead of a DSI as in Disco boards?

my stm32mp157f-dk2 board has a DSI (ECMF04-4HSWM10 filter) screen but my custom board is going to have a LVDS screen so what should I do different to protect the screen? (Filtering or ESD protection etc.)

This topic has been closed for replies.

2 replies

PatrickF
ST Employee
September 9, 2022

Hi @Gencay​ 

I added topic 'EMI Filtering and Signal Conditioning'

I assume you already have a DSI2LVDS converter (or RGB2LVDS brige), so question could be also for the bridge supplier.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
PatrickF
ST Employee
September 9, 2022

Hi,

I found that ECMF04-4HSWM10 could be used as for DSI (LVDS is lower requency than DSI).

ECMF04-4HSWM10 includes common mode filter for WLAN/BT bands.

For ESD protection only, HSP051-4M10 could be used instead (similar but not same footprint).

Maybe EMI/ESD experts might come with more suitable answer.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent