Skip to main content
Visitor II
October 23, 2023
Question

What is the highest version of opencv compatible with the gstreamer library included in this SDK?

I have transplanted the latest opencv-4.8.1 on the STM32MP135F-DK Discovery Board and run a program to capture video stream from a camera on the borad.
I found if I cmake the opencv-4.8.1 source code with "-DWITH_GSTREAMER=ON -DBUILD_GSTREAMER=ON",and when I am getting the camera data stream in the test program, the gstreamer library on the board reports the following error.

(opencv_camera:2589): GStreamer-CRITICAL **: 19:26:41.671: gst_sample_get_caps: assertion 'GST_IS_SAMPLE (sample)' failed
[ERROR:0@95.876] global cap_gstreamer.cpp:925 retrieveVideoFrame GStreamer: gst_sample_get_caps() returns NULL


Then I cmake the opencv-4.8.1 source code with "-DWITH_GSTREAMER=OFF -DBUILD_GSTREAMER=OFF", the errors are gone and the test program runs normally.

I think it might be that the opencv I compiled is not compatible with the gstreamer library included in the SDK.

Is my understanding right?

 

the version of the opencv I compiled:

opencv-4.8.1

the version of the gstreamer library included in the SDK:

libgstreamer-1.0.so.0.2200.0

SDK:

en.SDK-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz

My opencv cmake command

cmake -D WITH_IPP=OFF \
      -D BUILD_IPP=OFF \
      -D WITH_ADE=OFF \
      -D BUILD_ADE=OFF \
      -D WITH_GSTREAMER=ON \
      -D BUILID_GSTREAMER=ON \
      -D CMAKE_INSTALL_PREFIX=../install \
      ..

My test program

#include <iostream>

#include <opencv2/opencv.hpp>

using namespace std;
using namespace cv;

int main()
{
    VideoCapture cap(0);

    if (!cap.isOpened())
    {
        cout << "could not open the camera" << endl;
        return -1;
    }

    namedWindow("camera", WINDOW_AUTOSIZE);

    while (true)
    {
        Mat frame;

        cap >> frame;

        if (frame.empty())
            break;

        imshow("camera", frame);

        if (waitKey(30) == 'q')
            break;
    }

    cap.release();
    destroyAllWindows();

    return 0;
}

 

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
October 26, 2023

HI @babai50 ,

I have found v4.7.x is mention in this page : https://wiki.st.com/stm32mpu/wiki/Category:X-LINUX-AI_expansion_package#Contents

Regards

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent