Skip to main content
Associate III
December 16, 2020
Question

What is the cause of the error that occurs when loading the Cortex-M4 FW to the Cortex-A7 (Linux)?

We have confirmed the operation on our original board that

"STM32MP151CAA3" mounted on.

​

When I start our Cortex-A7 (Linux) FW and try to load our Cortex-M4 (RTOS: uC3) FW , an error message is output on the console of Linux.

​

The steps when an error occurs is described below.

Is there any possible cause for the error?

​

--Steps--

1) Write our Cortex-A7 (Linux) FW to a SD card and start it with our original board.

2) Build our Cortex-M4 (RTOS: uC3) FW. ⇒ Build is successful.

3) Transfer our Cortex-M4 (RTOS: uC3) FW to our original board by scp.

4) Start our Cortex-M4 (RTOS: uC3) FW by Cortex-A7 (Linux) FW.

⇒ Linux console shows the error message.

​

Best Regards,

H. Masuda

This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
December 16, 2020

Hi @HMasu.1​ ,

Did you check your M4 firmware runs ok in Engineering mode ?

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
HMasu.1Author
Associate III
December 17, 2020

Hi @Community member​ ,

​

Thank you for your reply.

I have checked in Engineering mode by using MDK Arm (uVision).

Loading M4 firmware is successful, but if I started program by step-in, suddenly the debugger disconnects when RTOS starts.

uVision don't show any message.

And I cannot get fault reports from uVision because the debugger disconnects.

Best Regards.

H. Masuda