Skip to main content
Dat Tran
Senior II
November 2, 2023
Question

What does "RCC_HSE_BYPASS_DIG" mean?

Hi, I see STM32MP1 - M4 use "RCC_HSE_BYPASS_DIG", what does this mean?

 

And from stm32mpcube, does anyone know the calculation below to get 209MHz?

 

 

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLL12SOURCE_HSE;

RCC_OscInitStruct.PLL.PLLM = 3;

RCC_OscInitStruct.PLL.PLLN = 81;

RCC_OscInitStruct.PLL.PLLP = 1;

RCC_OscInitStruct.PLL.PLLQ = 1;

RCC_OscInitStruct.PLL.PLLR = 1;

RCC_OscInitStruct.PLL.PLLFRACV = 0x800;

RCC_OscInitStruct.PLL.PLLMODE = RCC_PLL_FRACTIONAL;

RCC_OscInitStruct.PLL.RPDFN_DIS = RCC_RPDFN_DIS_DISABLED;

RCC_OscInitStruct.PLL.TPDFN_DIS = RCC_TPDFN_DIS_DISABLED;

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
November 6, 2023

Hi @Dat Tran 

RCC_HSE_BYPASS_DIG is to control the 'DIGBYP' in case there is an external oscillator instead of a crystal (which is the case on our EV1 and DK1/2 boards). Note that M4 does not need to control this unless in 'Engineering boot' (i.e. without Linux).

For PLL settings, you could use CubeMX clock configurator and look at generated code.
Otherwise, you should read the RCC section in Reference Manual.

PatrickF_0-1699279450587.png

 

Regards.

 

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent