Skip to main content
GWu.4
Associate
August 23, 2022
Solved

What data types are used for the fields in the STM header of binary files when the signature/sha256 is generated?

We are trying to verify the signature generated by the STM signing tool. From this link, in the table for "On STM32MP15x lines", we need to know what data type is used for each field when the signature hash (sha256) is created so we can replicate it.

This topic has been closed for replies.
OlivierK
OlivierKBest answer
ST Technical Moderator
September 5, 2022

Hi GWu.4 (Community Member)

For the bitfields did you have a look at the SigningTool page:

https://wiki.st.com/stm32mpu/wiki/Signing_tool

Using the help from the SigningTool command line version, you can also check all the data fields to be entered. For that you need to understand how the ROM code secure boot works and which algorithm are processed to authenticate and potentially decrypt a signed image.

https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_code_secure_boot#Image_signing

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

OlivierK
OlivierKBest answer
ST Technical Moderator
September 5, 2022

Hi GWu.4 (Community Member)

For the bitfields did you have a look at the SigningTool page:

https://wiki.st.com/stm32mpu/wiki/Signing_tool

Using the help from the SigningTool command line version, you can also check all the data fields to be entered. For that you need to understand how the ROM code secure boot works and which algorithm are processed to authenticate and potentially decrypt a signed image.

https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_code_secure_boot#Image_signing

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.