Skip to main content
NHuhs.2394
Associate II
Nov 23, 2020 1:26 PM UTC
Question

Use lan9303 in mdio mode on STM32MP157

Hi,

I am trying to use the lan9303 chip in mdio managed mode on a stm32mp157-based board.

I configured the Device tree according to https://kernel.googlesource.com/pub/scm/linux/kernel/git/next/linux-next/+/refs/heads/akpm-base/Documentation/devicetree/bindings/net/dsa/lan9303.txt

and my .dts file looks like this:

#include "stm32mp157.dtsi"
#include "stm32mp15xc.dtsi"
#include "stm32mp15-qsmp.dtsi"
 
 
/ {
	model = "Ka-Ro electronics GmbH QSMP-1570 module on HSW board v1";
	compatible = "karo,stm32mp157c-qsmp-1570", "st,stm32mp157";
};
 
&gpu {
	status = "okay";
};
 
 
 
 
 
&ethernet0 {
 status = "okay";
 pinctrl-0 = <&ethernet0_rmii_pins_a>;
 pinctrl-1 = <&ethernet0_rmii_pins_sleep_a>;
 pinctrl-names = "default", "sleep";
	phy-mode = "rmii";
	max-speed = <1000>;
 
	phy-handle = <&switch>;
	mdio0 {
		#address-cells = <1>;
		#size-cells = <0>;
 compatible = "snps,dwmac-mdio";
 
 
 
			switch: switch-phy@0 {
					compatible = "smsc,lan9303-mdio";
					reg = <0>;
 
 
					ports {
						#address-cells = <1>;
						#size-cells = <0>;
 
						port@0 {
							reg = <0>;
							label = "cpu";
							ethernet = <&ethernet0>;
						};
 
						port@1 { /* external port 1 */
							reg = <1>;
							label = "lan1";
						};
 
						port@2 { /* external port 2 */
							reg = <2>;
							label = "lan2";
						};
					};
				};
		};
					
				
};

On boot the kernel recognizes the lan9303 driver and the ports lan1 and lan2 but fails to find a PHY. I will attach the output.

The ethernet node in the flattened device tree looks like this:

ethernet@5800a000 {
 compatible = "st,stm32mp1-dwmac", "snps,dwmac-4.20a";
 reg = <0x5800a000 0x00002000>;
 reg-names = "stmmaceth";
 interrupts = <0x00000000 0x0000003d 0x00000004>;
 interrupt-names = "macirq";
 clock-names = "stmmaceth", "mac-clk-tx", "mac-clk-rx", "eth-ck", "ethstp";
 clocks = <0x00000004 0x00000069 0x00000004 0x00000067 0x00000004 0x00000068 0x00000004 0x0 000007b 0x00000004 0x00000070>;
 st,syscon = <0x00000003 0x00000004>;
 snps,mixed-burst;
 snps,pbl = <0x00000002>;
 snps,en-tx-lpi-clockgating;
 snps,axi-config = <0x00000028>;
 snps,tso;
 status = "okay";
 pinctrl-names = "default", "sleep";
 pinctrl-0 = <0x00000029>;
 pinctrl-1 = <0x0000002a>;
 phy-handle = <0x0000002b>;
 phy-mode = "rmii";
 max-speed = <0x000003e8>;
 phandle = <0x0000002d>;
 mdio0 {
 #address-cells = <0x00000001>;
 #size-cells = <0x00000000>;
 compatible = "snps,dwmac-mdio";
 reset-gpios = <0x0000002c 0x00000004 0x00000001>;
 reset-delay-us = <0x00002710>;
 post-reset-delay-us = <0x000003e8>;
 ethernet-phy@3 {
 compatible = "ethernet-phy-id0022.1622";
 reg = <0x00000003>;
 interrupt-parent = <0x0000002c>;
 interrupts = <0x00000009 0x00000002>;
 rxd0-skew-ps = <0x000001aa>;
 rxd1-skew-ps = <0x000001a9>;
 rxd2-skew-ps = <0x000001a3>;
 rxd3-skew-ps = <0x0000018e>;
 txd0-skew-ps = <0x0000013d>;
 txd1-skew-ps = <0x0000013c>;
 txd2-skew-ps = <0x0000015b>;
 txd3-skew-ps = <0x0000018b>;
 txen-skew-ps = <0x000001b3>;
 rxdv-skew-ps = <0x00000198>;
 rxc-skew-ps = <0x00000384>;
 txc-skew-ps = <0x0000076c>;
 };
 switch-phy@0 {
 compatible = "smsc,lan9303-mdio";
 reg = <0x00000000>;
 phandle = <0x0000002b>;
 ports {
 #address-cells = <0x00000001>;
 #size-cells = <0x00000000>;
 port@0 {
 reg = <0x00000000>;
 label = "cpu";
 ethernet = <0x0000002d>;
 };
 port@1 {
 reg = <0x00000001>;
 label = "lan1";
 };
 port@2 {
 reg = <0x00000002>;
 label = "lan2";
 };
 };
 };
 };
 };

I checked all the Pin connections and everything seems to be ok.

Does anybody have any experience with the lan9303 Chip in mdio-managed mode?

Thanks in advance

This topic has been closed for replies.

9 replies

Christophe Guibout
ST Technical Moderator
Nov 27, 2020 1:24 PM UTC

Hi @NHuhs.2394​ ,

In your log, it seems that an interrupt-names is missing :

[ 4.349668] stm32-dwmac 5800a000.ethernet: IRQ eth_wake_irq not found

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NHuhs.2394
Associate II
Nov 30, 2020 11:03 AM UTC

Hi Christophe,

I added the interrupt following the guide at : https://wiki.st.com/stm32mpu/wiki/Ethernet_device_tree_configuration#RMII_with_Crystal_on_PHY_-28Reference_clock_-28standard_RMII_clock_name-29_is_provided_by_a_Phy_Crystal-29

Still no success.

Still getting a message about a missing interrupt, but this one shouldn't be needed. And the Eth_Clock should be provided by the lan chip.

I read in another forum, that some ST Boards have PHY Address 0 reserved for internal purposes.

DOes somebody know if thats the case for the STM32MP157c?(I couldn't find anything) In that case I would have to change my Board layout.

Christophe Guibout
ST Technical Moderator
Nov 30, 2020 12:23 PM UTC

Hi @NHuhs.2394​ ,

By having a look into your log, ethernet seems broken even at u-boot stage:

Net: MAC addr from fuse: 00:0c:c6:88:4f:bc
ethernet@5800a000: EQOS_DMA_MODE_SWR stuck
No ethernet found.

Before investigating the issue on the kernel, I would recommand to fix the one from u-boot, or temporally disable ethernet feature in u-boot. Then ethernet from kernel will be able to init from an HW clean state.

I didn't see any reset entry in your node : how is manage the reset of the switch ?

In the documentation, it's managed like that:

reset-gpios = <&gpio7 6 GPIO_ACTIVE_LOW>;
reset-duration = <200>;

Could you also please tell me on which MMDV version you are ? (MMDV-1.x.x or MMDV-2.x.x ?)

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NHuhs.2394
Associate II
Nov 30, 2020 1:34 PM UTC

Thanks, I will try to disable ethernet in u-boot. Do you know if its possible to do it directly in u-boot or do I have to modify the Code/Device Tree?

The Reset of the switch is directly connected to a reset button. Not to any GPIO. The reset-gpios parameter is called "optional" in the doc, and it seemed to work on similar boards.

I am sorry but I don't know what you mean with MMDV.

MWoło.1
Associate
Nov 8, 2021 12:33 PM UTC

The problem was solved? Can You add some comments?

NHuhs.2394
Associate II
Nov 10, 2021 8:28 AM UTC

Yes the problem was solved.

What I did was following things:

  • In the u-boot defconfig I disabled Ethernet
  • In the linux-kernel config (via menuconfig) I under Device Drivers > Network Device Support > Ethernet Driver Support I used the generic driver for DWMAC
  • DTS configuration for ethernet looks like this:
&ethernet0 {
 status = "okay";
 pinctrl-0 = <&ethernet0_rmii_pins_a>;
 pinctrl-1 = <&ethernet0_rmii_pins_sleep_a>;
 pinctrl-names = "default", "sleep";
	phy-mode = "rmii";
};
 
 
 
&pinctrl {
	ethernet0_rmii_pins_a: rmii-0 {
		pins1 {
			pinmux = <STM32_PINMUX('G', 13, AF11)>, /* ETH1_RMII_TXD0 */
				 <STM32_PINMUX('G', 14, AF11)>, /* ETH1_RMII_TXD1 */
				 <STM32_PINMUX('B', 11, AF11)>, /* ETH1_RMII_TX_EN */
				 <STM32_PINMUX('A', 1, AF11)>, /* ETH1_RMII_REF_CLK */
				 <STM32_PINMUX('A', 2, AF11)>, /* ETH1_MDIO */
				 <STM32_PINMUX('C', 1, AF11)>; /* ETH1_MDC */
			bias-disable;
			drive-push-pull;
			slew-rate = <2>;
		};
		pins2 {
			pinmux = <STM32_PINMUX('C', 4, AF11)>, /* ETH1_RMII_RXD0 */
				 <STM32_PINMUX('C', 5, AF11)>, /* ETH1_RMII_RXD1 */
				 <STM32_PINMUX('A', 7, AF11)>; /* ETH1_RMII_CRS_DV */
			bias-disable;
		};
	};
 
	ethernet0_rmii_pins_sleep_a: rmii-sleep-0 {
		pins1 {
			pinmux = <STM32_PINMUX('G', 13, ANALOG)>, /* ETH1_RMII_TXD0 */
				 <STM32_PINMUX('G', 14, ANALOG)>, /* ETH1_RMII_TXD1 */
				 <STM32_PINMUX('B', 11, ANALOG)>, /* ETH1_RMII_TX_EN */
				 <STM32_PINMUX('A', 2, ANALOG)>, /* ETH1_MDIO */
				 <STM32_PINMUX('C', 1, ANALOG)>, /* ETH1_MDC */
				 <STM32_PINMUX('C', 4, ANALOG)>, /* ETH1_RMII_RXD0 */
				 <STM32_PINMUX('C', 5, ANALOG)>, /* ETH1_RMII_RXD1 */
				 <STM32_PINMUX('A', 1, ANALOG)>, /* ETH1_RMII_REF_CLK */
				 <STM32_PINMUX('A', 7, ANALOG)>; /* ETH1_RMII_CRS_DV */
		};
	};
 
 
 
};
  • DTS configuration for phy looks like this:
&mdio0 {
	reset-gpios = <&gpioa 4 GPIO_ACTIVE_LOW>;
	reset-delay-us = <10000>;
	post-reset-delay-us = <1000>;
 
	phy0: ethernet-phy@0 {
		compatible = "ethernet-phy-id0022.1622";
		reg = <0>;
	};
};

The lan9303 acts as a switch and I am able to use both LAN-Ports .

MWoło.1
Associate
Nov 10, 2021 8:43 AM UTC

Thanks a lot, I try it. The reset is mandatory?

Best Regards

MWoło.1
Associate
Nov 10, 2021 3:03 PM UTC

I have a follwing error

[ 2.816259] stm32-dwmac 5800a000.ethernet: IRQ eth_lpi not found
[ 2.821084] stm32-dwmac 5800a000.ethernet: PTP uses main clock
[ 2.826849] stm32-dwmac 5800a000.ethernet: no reset control found
[ 2.833593] stm32-dwmac 5800a000.ethernet: User ID: 0x40, Synopsys ID: 0x42
[ 2.839981] stm32-dwmac 5800a000.ethernet: DWMAC4/5
[ 2.845039] stm32-dwmac 5800a000.ethernet: DMA HW capability register supported
[ 2.852384] stm32-dwmac 5800a000.ethernet: RX Checksum Offload Engine supported
[ 2.859817] stm32-dwmac 5800a000.ethernet: TX Checksum insertion supported
[ 2.866775] stm32-dwmac 5800a000.ethernet: Wake-Up On Lan supported
[ 2.873222] stm32-dwmac 5800a000.ethernet: TSO supported
[ 2.878443] stm32-dwmac 5800a000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 2.886415] stm32-dwmac 5800a000.ethernet: device MAC address 32:a1:b4:b2:49:cf
[ 2.893792] stm32-dwmac 5800a000.ethernet: Enabled Flow TC (entries=2)
[ 2.900364] stm32-dwmac 5800a000.ethernet: TSO feature enabled
[ 2.906287] stm32-dwmac 5800a000.ethernet: Using 32 bits DMA width
[ 44.658224] using random self ethernet address
[ 44.661279] using random host ethernet address
[ 45.253396] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [Generic PHY] (irq=POLL)
[ 46.283123] stm32-dwmac 5800a000.ethernet: Failed to reset the dma
[ 46.287939] stm32-dwmac 5800a000.ethernet eth0: stmmac_hw_setup: DMA engine initialization failed
[ 46.313146] stm32-dwmac 5800a000.ethernet eth0: stmmac_open: Hw setup failed

but is much better I have before

MWoło.1
Associate
Nov 13, 2021 2:37 PM UTC

After some modification I get

[ 3.039706] libphy: stmmac: probed
[ 3.041706] mdio_bus stmmac-0:00: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:00, irq=POLL)
[ 3.051566] SMSC LAN911x Internal PHY stmmac-0:01: attached PHY driver [SMSC LAN911x Internal PHY] (mii_bus:phy_addr=stmmac-0:01, irq=POLL)
[ 3.064334] SMSC LAN911x Internal PHY stmmac-0:02: attached PHY driver [SMSC LAN911x Internal PHY] (mii_bus:phy_addr=stmmac-0:02, irq=POLL)
[ 3.076816] mdio_bus stmmac-0:10: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:10, irq=POLL)
[ 3.086446] mdio_bus stmmac-0:11: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:11, irq=POLL)
[ 3.096064] mdio_bus stmmac-0:12: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:12, irq=POLL)
[ 3.105695] mdio_bus stmmac-0:13: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:13, irq=POLL)
[ 3.115341] mdio_bus stmmac-0:14: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:14, irq=POLL)
[ 3.124960] mdio_bus stmmac-0:15: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:15, irq=POLL)
[ 3.134592] mdio_bus stmmac-0:16: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:16, irq=POLL)
[ 3.144235] mdio_bus stmmac-0:17: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:17, irq=POLL)
[ 3.153857] mdio_bus stmmac-0:18: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:18, irq=POLL)
[ 3.163489] mdio_bus stmmac-0:19: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:19, irq=POLL)
[ 3.173122] mdio_bus stmmac-0:1a: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:1a, irq=POLL)
[ 3.182739] mdio_bus stmmac-0:1b: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:1b, irq=POLL)
[ 3.192386] mdio_bus stmmac-0:1c: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:1c, irq=POLL)
[ 3.202024] mdio_bus stmmac-0:1d: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:1d, irq=POLL)
[ 3.211675] mdio_bus stmmac-0:1e: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:1e, irq=POLL)
[ 3.221290] mdio_bus stmmac-0:1f: attached PHY driver [unbound] (mii_bus:phy_addr=stmmac-0:1f, irq=POLL)
[ 16.953699] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [Generic PHY] (irq=POLL)
[ 17.987895] stm32-dwmac 5800a000.ethernet eth0: stmmac_hw_setup: DMA engine initialization failed
[ 18.013087] stm32-dwmac 5800a000.ethernet eth0: stmmac_open: Hw setup failed

Still the same problem with DMA. What is missing, which clock is missing?