Skip to main content
Associate
May 8, 2024
Question

USB C connection problem with MP151cad3.

Dear. All.

I have one problem.

until now, I used well to connect with USB OTG interface.

I've been using USB C to USB A cable. and then, we have no problem.

but, I found a problem at using USB C to USB C connectivity.

the PC & my MP151C board didn't recognize each other.

I'll use my device for slave.

our circuit as bellow.

thank you.

Geonbangjini_0-1715164396958.png

 

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
July 8, 2024

Hi @Geonbangjini 

ID pin is useless for USB Type-C, the concept does not exist.

CC1/CC2 lines should have each a 5.1K pull-dow to be recognized as a slave device by the Host PC.

 

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent