Skip to main content
SAman.1
Associate III
February 27, 2021
Question

USART3 platform_get_irq faild

  • February 27, 2021
  • 1 reply
  • 4357 views

Hy i am using the usart3 from the STM32MP157A-DK1. i orientated myself on the USART driver (https://elixir.bootlin.com/linux/latest/source/drivers/tty/serial/stm32-usart.c).

but

when i want to initialize the

port I get following error code “Rs453Network: probe of 4000f000.serial failed

with error 77�? on this methode stm32port->wakeirq = platform_get_irq(pdev, 1);

I have this device tree configuration:

Stm32mp15xx-dkx.dtsi

&usart3 {

               pinctrl-names = "default", "sleep", "idle";

               pinctrl-0 = <&usart3_pins_b>;

               pinctrl-1 = <&usart3_sleep_pins_b>;

               pinctrl-2 = <&usart3_idle_pins_b>;

               uart-has-rtscts;

               status = "okay";

};

Stm32mp157a-dk1.dts

aliases {

                               ethernet0 = &ethernet0;

                               serial0 = &uart4;

                               //serial1 = &usart3;

                               serial2 = &uart7;

                               usart3 = &usart3;

               };

this is the methode:

static int stm32_init_port(struct stm32_port *stm32port,

 struct platform_device *pdev)

{

struct uart_port *port = &stm32port->port;

struct resource *res;

int ret;

port->iotype = UPIO_MEM;

port->flags = UPF_BOOT_AUTOCONF;

port->ops = &stm32_uart_ops;

port->dev = &pdev->dev;

port->fifosize = stm32port->info->cfg.fifosize;

   

   

ret = platform_get_irq(pdev, 0); //get an IRQ for a device

if (ret <= 0)

return ret ? : -ENODEV;

port->irq = ret;

port->rs485_config = stm32_config_rs485;

   

stm32_init_rs485(port, pdev);

if (stm32port->info->cfg.has_wakeup) {

stm32port->wakeirq = platform_get_irq(pdev, 1);

if (stm32port->wakeirq <= 0 && stm32port->wakeirq != -ENXIO)

      return stm32port->wakeirq ? : -ENODEV;

}

stm32port->fifoen = stm32port->info->cfg.has_fifo;

  /*get information on the structure of the device resource, 

  like start adress and end adress, in order to find the 

  resource memory size so you can map it in memory.*/

res = platform_get_resource(pdev, IORESOURCE_MEM, 0);

port->membase = devm_ioremap_resource(&pdev->dev, res);

if (IS_ERR(port->membase))

    return PTR_ERR(port->membase);

     

port->mapbase = res->start;

spin_lock_init(&port->lock);

stm32port->clk = devm_clk_get(&pdev->dev, NULL);

if (IS_ERR(stm32port->clk))

return PTR_ERR(stm32port->clk);

/* Ensure that clk rate is correct by enabling the clk */

ret = clk_prepare_enable(stm32port->clk);

if (ret)

return ret;

stm32port->port.uartclk = clk_get_rate(stm32port->clk);

if (!stm32port->port.uartclk) {

clk_disable_unprepare(stm32port->clk);

ret = -EINVAL;

}

return ret;

}

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
March 8, 2021
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent