Skip to main content
Associate II
Mar 5, 2026 6:58 AM UTC
Question

Usage of M33 core in standalone mode in stm32mp257

Hi,

Can I use only M33 core as a standalone controller on stm32mp257 evaluation board without need of linux operating system and DDR

1 reply

PatrickF
ST Employee
Mar 5, 2026 9:05 AM UTC

Hi @srisatya2007 

This is what we name M33-TD, where Linux on A35 is optional (then you should question choice of STM32MP2 for only M33 core).

Please look to https://wiki.st.com/stm32mpu/wiki/How_to_migrate_STM32CubeMPU_examples_from_A35-TD_flavor_to_M33-TD_flavor

and https://wiki.st.com/stm32mpu/wiki/STM32MP2_boot_chain_overview#STM32MP2_M33-TD_flavor_boot_chain

 

In our SW deliveries, DDR is assumed mandatory due to limited internal RAM size and our default choice of having M33 TF-M and application code copied from external Flash to DDR instead of XiP (because XiP is limited to Serial-Flash/RAM and not possible on eMMC or SD-Card).
But you could probably build you SW differently (then with limited ST support).

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent