Skip to main content
SMich.1
Senior
August 24, 2020
Solved

update STM32CubeIDE Version: 1.4.2 stopped sending Firmware to MPU

  • August 24, 2020
  • 9 replies
  • 3404 views

hi,

i updated STM32CubeIDE

to

Version: 1.4.2

Build: 7643_20200813_1322 (UTC)

and now the debug session doesn't send the compiled firmware to the target and just starts the gdb connection :

Open On-Chip Debugger 0.10.0+dev-g30d1303 (2020-06-18-09:13)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : STLINK V2J37M26 (API v2) VID:PID 0483:3752

Info : Target voltage: 3.198425

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : clock speed 4000 kHz

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x6ba02477

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x6ba02477

Info : STM32MP157CAAx.cm4: hardware has 6 breakpoints, 4 watchpoints

Info : STM32MP157CAAx.cpu0: hardware has 6 breakpoints, 4 watchpoints

Info : STM32MP157CAAx.cpu1: hardware has 6 breakpoints, 4 watchpoints

Info : STM32MP157CAAx.cm4: external reset detected

Info : starting gdb server for STM32MP157CAAx.cpu0 on 3334

Info : Listening on port 3334 for gdb connections

Info : starting gdb server for STM32MP157CAAx.cm4 on 3333

Info : Listening on port 3333 for gdb connections

Info : accepting 'gdb' connection on tcp/3333

Info : Halt timed out, wake up GDB.

Error: timed out while waiting for target halted

Error executing event gdb-attach on target STM32MP157CAAx.cm4:

Info : New GDB Connection: 1, Target STM32MP157CAAx.cm4, state: reset

Warn : negative reply, retrying

Warn : negative reply, retrying

Warn : target not halted

Info : target STM32MP157CAAx.cm4 was not halted when resume was requested

Info : The target is not running when halt was requested, stopping GDB.

Warn : target STM32MP157CAAx.cm4 is not halted (gdb fileio)

Warn : target not halted

shutdown command invoked

Info : dropped 'gdb' connection

How can i fix that?

This topic has been closed for replies.
Best answer by Olivier GALLIEN

Hi @SMich.1​ 

Sorry for inconvenience. This is a identified issue in our latest delivery.

As per already reported in previous post https://community.st.com/s/question/0D53W00000DGXEXSA5/stm32cubeide-debugger-wont-work-with-stm32mp1-dk2-with-the-20-dunfell-release

​The fix is now published.

https://wiki.st.com/stm32mpu/wiki/STM32MP15_ecosystem_release_note_-_v2.0.0

https://wiki.st.com/stm32mpu/wiki/STM32MP15_OpenSTLinux_release_note_-_v2.0.0

some cipher methods have been disabled by the community for security reasons.

As a consequence some ssh requests from STM32CubeIDE may not be functional due to the dropbear package configuration.

In this case, you can either:

Olivier

9 replies

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
August 24, 2020

Hi @SMich.1​ 

Sorry for inconvenience. This is a identified issue in our latest delivery.

As per already reported in previous post https://community.st.com/s/question/0D53W00000DGXEXSA5/stm32cubeide-debugger-wont-work-with-stm32mp1-dk2-with-the-20-dunfell-release

​The fix is now published.

https://wiki.st.com/stm32mpu/wiki/STM32MP15_ecosystem_release_note_-_v2.0.0

https://wiki.st.com/stm32mpu/wiki/STM32MP15_OpenSTLinux_release_note_-_v2.0.0

some cipher methods have been disabled by the community for security reasons.

As a consequence some ssh requests from STM32CubeIDE may not be functional due to the dropbear package configuration.

In this case, you can either:

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SMich.1
SMich.1Author
Senior
August 24, 2020

so the problem are in dunfell release ? not in the ide ?

I building dunfell for custom machine so if i understand right i should add to the dropbear : PACKAGECONFIG_remove = "disable-weak-ciphers"PR = "r1" ?

Olivier GALLIEN
ST Technical Moderator
August 24, 2020

It's an unforeseen compability break between STM32CubeIDE and dunfell.

Waiting for proper fix in STM32CubeIDE we have temporary decided to workaround this on dunfell side. ( faster)

Seems you understand correctly patch to apply to your distribution.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SMich.1
SMich.1Author
Senior
August 24, 2020

tnx, worked

AZele.2
Visitor II
August 31, 2020

Hi,

I have a similar problem.

I try run example from wiki for STM32MP157C-DK2: OpenAMP_TTY_echo.

This is my log from CubeIDE (ver. 1.4.0)

----------------------------------------------------------------------------------------------------

Open On-Chip Debugger 0.10.0+dev-g30d1303 (2020-06-18-09:11)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : STLINK V2J37M26 (API v2) VID:PID 0483:3752

Info : Target voltage: 3.217357

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : clock speed 4000 kHz

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x6ba02477

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x6ba02477

Info : STM32MP157CAAx.cm4: hardware has 6 breakpoints, 4 watchpoints

Info : STM32MP157CAAx.cpu0: hardware has 6 breakpoints, 4 watchpoints

Info : STM32MP157CAAx.cpu1: hardware has 6 breakpoints, 4 watchpoints

Info : STM32MP157CAAx.cm4: external reset detected

Info : starting gdb server for STM32MP157CAAx.cpu0 on 3334

Info : Listening on port 3334 for gdb connections

Info : starting gdb server for STM32MP157CAAx.cm4 on 3333

Info : Listening on port 3333 for gdb connections

Info : accepting 'gdb' connection on tcp/3333

Info : Halt timed out, wake up GDB.

Error: timed out while waiting for target halted

Error executing event gdb-attach on target STM32MP157CAAx.cm4:

Info : New GDB Connection: 1, Target STM32MP157CAAx.cm4, state: reset

Warn : negative reply, retrying

Warn : negative reply, retrying

Warn : target not halted

Info : target STM32MP157CAAx.cm4 was not halted when resume was requested

Warn : target not halted

shutdown command invoked

Info : dropped 'gdb' connection

----------------------------------------------------------------------------------------------------

1. I use the latest STM32MP1_Starter_Package_-_images: en.FLASH-stm32mp1-openstlinux-5-4-dunfell-mp1-20-06-24.tar.xz (FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv).

2. I update the drobpear package on the STM32MP1 board:

----------------------------------------------------------------------------------------------

root@stm32mp1:~# apt-cache policy dropbear

dropbear:

 Installed: 2019.78-r2

 Candidate: 2019.78-r2

 Version table:

 *** 2019.78-r2 500

    500 http://packages.openstlinux.st.com/2.0 dunfell/updates armhf Packages

    100 /var/lib/dpkg/status

----------------------------------------------------------------------------------------------

But I can not sending Firmware to MPU.

How do I run this example from the wiki

SMich.1
SMich.1Author
Senior
August 31, 2020

You sure 2019.78-r2 that this is the version with update?

AZele.2
Visitor II
August 31, 2020

Yes. I use commands from release note: https://wiki.st.com/stm32mpu/wiki/STM32MP15_ecosystem_release_note_-_v2.0.0#Main_restrictions (5.1.1 OpenSTLinux (Cortex®-A7)).

Before update was:

Installed: 2019.78-r1

Candidate: 2019.78-r2

Olivier GALLIEN
ST Technical Moderator
August 31, 2020

Hi @AZele.2​ 

It should work properly with the 2019.78-r1 integrated by default.

Did you/could you test it ?

I will have a further look for the issue with r2.

Thx

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
AZele.2
Visitor II
September 1, 2020

I solved part of the problem after installing CubeIde 1.4.0 on Windows 7 operating system (all work).

Before that I used Ubuntu 18.04 (Virtual Box)

It looks like a problem in using Virtual Box.