Skip to main content
YRink.1
Associate II
February 5, 2021
Question

Understanding the functions of Remoteproc

Hi,

iam a bit confused aboute the remoteproc framework and if my understanding of it is correct.

In my view, the remoteproc framework can start the m3 firmware with having its elf-file in a dedicated place of the filesystem. The remoteproc also parses the resource table of the m3 and allocates the memory which is specified for the vrings etc, that a communication can be established in a shared memory. But i have few problems with understanding the stop and shutdown commando from remoteproc. Are those commands just associated with the stm32_rproc driver. What happens with the m3 when i call the remoteproc stop and shutdown. Does the stm32_rpoc driver just shutdown the clocks and voltages for the m3. And how it can resume them without loading the elf file again? Does it just trigger an wake-up source if i wanna have th m3 active via the command start again and it resumes the code in the elf file?

This topic has been closed for replies.

1 reply

Olivier GALLIEN
ST Technical Moderator
February 8, 2021

Hi @Community member​ ,

Based on this article :

https://wiki.st.com/stm32mpu/wiki/Linux_remoteproc_framework_overview

"Stop" reset the coproc ( no action on clocks and voltage which are shared with A7 ), "Start" reload the firmware in MCURAM from Linux filesystem and start coproc.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.