Skip to main content
mfny
Associate II
Mar 22, 2025 10:21 PM UTC
Question

Unable to program STM32MP257F-DK

Hi all, having an issue with programming STM32MP257F-DK/SDCard with the Starter package getting to the stage in the attached screenshot then it seems a connection times out with no success notification popup ?

This topic has been closed for replies.

6 replies

ST Technical Moderator
Mar 25, 2025 12:47 PM UTC

Hello @mfny,

 

Perhaps this is due to an insufficient power supply.

How do you power the board? The recommended power supply is a USB-C/USB-C 5V/3A cable as shown in https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards/STM32MP257x-DK/Let%27s_start/Unpack_the_STM32MP257x-DK_board#Required_equipment

 

If changing to a USB-C 5V/3A cable doesn't solve anything, can you send the whole STM32CubeProgrammer log to investigate further ?

 

Kind regards,
Thomas

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
mfny
mfnyAuthor
Associate II
Mar 26, 2025 3:16 PM UTC

Hello.

How would I obtain the full log to send ?

ST Technical Moderator
Mar 26, 2025 3:53 PM UTC

Hello,

In STM32CubeProgrammer there is a floppy disk icon on the right of the log section, you just have to click on it to save the logs.

 

Kind regards,
Thomas

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
mfny
mfnyAuthor
Associate II
Mar 26, 2025 6:26 PM UTC

Attached is a log file in a zip from STM32CubeProgrammer with Verbose set to 3. Also there is now no Timeout Error being shown but flashing is stuck at 100% progress with no error messages and there is a Blue led lit on the board.

mfny
mfnyAuthor
Associate II
Apr 6, 2025 9:22 PM UTC

Has anyone been able to look at the log I posted and can offer a solution to this issue ?

PatrickF
ST Employee
Apr 7, 2025 6:40 AM UTC

Hi,

this sound like a classic pitfall when the board starts uBoot, then USB DFU (from BootROM) is disconnected and a new USB DFU is setup by uBoot.

If you are using a Linux Virtual Machine, check (once flashing has failed) if the 'new' USB is visible to the Virtual Machine and not by Windows. There should be some settings in your VM to control that behavior.

Fixed Blue led mean uBoot is started correctly.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent