Skip to main content
Associate III
April 3, 2024
Solved

Unable to find the partition with the uuid mentioned in metadata

Hello everyone,

we have developed a custom board based on stm32mp157 chip. We also forked the tf-a and u-boot from meta-st layer. If we flash an sd card using the flash layout, image works. But my goal is to copy the files from linux host machine, which I did. Now the image does not boot from the sd card. It is showing following error.

NOTICE: CPU: STM32MP157CAA Rev.Z
NOTICE: Model: emtrion DIMM-Argon stm32mp157c, yocto, SDCARD
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using EMMC
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.6-stm32mp1-r2.0(debug):v2.6-dirty(a1f02f4f)
NOTICE: BL2: Built : 13:14:26, Nov 23 2021
ERROR: Unable to find the partition with the uuid mentioned in metadata

Does anyone have any idea, how to solve this? THANKS IN ADVANCE.

This topic has been closed for replies.
PatrickD
PatrickDBest answer
ST Employee
April 4, 2024

Hi,

UUID of the GPT partitions are used in TF-A to select the FIP partitions, these UUID information is used in "metadata" used of TFA secure udpate as decrivbe in https://wiki.st.com/stm32mpu/wiki/Secure_Firmware_Update

You need also to select the correct Type UID for FIP

 

See also https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#Block_device_GPT_partition-_SD_card_-2F_e-E2-80-A2MMC


The expected UUID for STM32MP1 board can be found in WIKI

https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#GPT_partuuid_of_FIP_partition

 

on Linux you can define the UID when you create the GPT partition, when you use gdisk:

on modify later for example with sgdisk

-t, --typecode=partnum:{hexcode|GUID}Change a single partition's type code. You enter the type code using either a two-byte hexadecimal number, as described earlier, or a fully-specified GUID value, such as EBD0A0A2-B9E5-4433-87C0-68B6B72699C7.

-u, --partition-guid=partnum:guidSet the partition unique GUID for an individual partition. The GUID may be a complete GUID or 'R' to set a random GUID.

 

You can check also the script for example.

https://github.com/STMicroelectronics/meta-st-stm32mp/blob/mickledore/recipes-devtools/sdcard-raw-tools/sdcard-raw-tools/create_sdcard_from_flashlayout.sh

 


DEFAULT_FIP_TYPEUUID=19d5df83-11b0-457b-be2c-7559c13142a5
DEFAULT_FIP_A_PARTUUID=4fd84c93-54ef-463f-a7ef-ae25ff887087
DEFAULT_FIP_B_PARTUUID=09c54952-d5bf-45af-acee-335303766fb3

Regards 

Patrick

 

  

1 reply

PatrickD
PatrickDBest answer
ST Employee
April 4, 2024

Hi,

UUID of the GPT partitions are used in TF-A to select the FIP partitions, these UUID information is used in "metadata" used of TFA secure udpate as decrivbe in https://wiki.st.com/stm32mpu/wiki/Secure_Firmware_Update

You need also to select the correct Type UID for FIP

 

See also https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#Block_device_GPT_partition-_SD_card_-2F_e-E2-80-A2MMC


The expected UUID for STM32MP1 board can be found in WIKI

https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#GPT_partuuid_of_FIP_partition

 

on Linux you can define the UID when you create the GPT partition, when you use gdisk:

on modify later for example with sgdisk

-t, --typecode=partnum:{hexcode|GUID}Change a single partition's type code. You enter the type code using either a two-byte hexadecimal number, as described earlier, or a fully-specified GUID value, such as EBD0A0A2-B9E5-4433-87C0-68B6B72699C7.

-u, --partition-guid=partnum:guidSet the partition unique GUID for an individual partition. The GUID may be a complete GUID or 'R' to set a random GUID.

 

You can check also the script for example.

https://github.com/STMicroelectronics/meta-st-stm32mp/blob/mickledore/recipes-devtools/sdcard-raw-tools/sdcard-raw-tools/create_sdcard_from_flashlayout.sh

 


DEFAULT_FIP_TYPEUUID=19d5df83-11b0-457b-be2c-7559c13142a5
DEFAULT_FIP_A_PARTUUID=4fd84c93-54ef-463f-a7ef-ae25ff887087
DEFAULT_FIP_B_PARTUUID=09c54952-d5bf-45af-acee-335303766fb3

Regards 

Patrick