Hello @BillR ,
I made some test on my 157c-dk2 board and it works.
The name of my new dts is "stm32mp157c-dk2-test.dts", it is just a copy of "stm32mp157c-dk2.dts".
I didn't modified the "compatible" property, it is still:
compatible = "st,stm32mp157c-dk2", "st,stm32mp157";
Please can you verify that you also made a copy of the u-boot.dtsi file with the same name?
[osboxes@osboxes ...es/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2/arch/arm/dts]
$ ll stm32mp157c-dk2*
-rw-rw-r-- 1 osboxes osboxes 119378 Apr 15 06:47 stm32mp157c-dk2.dtb
-rw-r--r-- 1 osboxes osboxes 2918 Apr 14 14:10 stm32mp157c-dk2.dts
-rw-rw-r-- 1 osboxes osboxes 119378 Apr 15 07:22 stm32mp157c-dk2-test.dtb
-rw-r--r-- 1 osboxes osboxes 2918 Apr 14 14:10 stm32mp157c-dk2-test.dts
-rw-r--r-- 1 osboxes osboxes 139 Apr 15 06:46 stm32mp157c-dk2-test-u-boot.dtsi
-rw-r--r-- 1 osboxes osboxes 139 Oct 18 13:27 stm32mp157c-dk2-u-boot.dtsi
You can see in the ls -l above that I have a:
- stm32mp157c-dk2-test.dts
- stm32mp157c-dk2-test-u-boot.dtsi
The u-boot.dtsi file is important because it is automatically included in the dts file with the same name.
This behavior is explained in the wiki: https://wiki.st.com/stm32mpu/wiki/STM32MP15_U-Boot#STM32MP15x_lines_support
-----------------------
You can use the command dtc, to verify that your dtb is correct without flashing your board.
dtc arch/arm/dts/stm32mp157c-dk2.dtb > dtc-stm32mp157c-dk2.dts
dtc arch/arm/dts/stm32mp157c-dk2-test.dtb > dtc-stm32mp157c-dk2-test.dts
The command "dtc" convert a generated dtb in a big dts file. This command is very helpful to verity the content of your final DTB, because all the include files have already been processed.
Once converted your two DTB files in dts, you can then verify that they are identical:
diff dtc-stm32mp157c-dk2.dts dtc-stm32mp157c-dk2-test.dts
or by using a diff tool like "meld".
Hope it helps,
Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.