Skip to main content
KKett.1
Associate
July 22, 2020
Question

Trying to attach a TI DP83848CVV PHY to STM32MP157 with external 50MHZ

Hello,

i'm currently trying to attach a TI DP83848CVV phy to the STM32MP157. We have an external 50MHZ clock which is supplied to the PHY and PA1 (ETH1_REF_CLK).

These are the pinctrl values (generated by CubeMX):

ethernet0_rmii_pins: rmii-0 {
		pins1 {
				pinmux = <STM32_PINMUX('A', 1, AF11)>, /* ETH1_REF_CLK */
						 <STM32_PINMUX('B', 12, AF11)>, /* ETH1_TXD0 */
						 <STM32_PINMUX('C', 1, AF11)>, /* ETH1_MDC */
						 <STM32_PINMUX('G', 14, AF11)>; /* ETH1_TXD1 */
				bias-disable;
				drive-push-pull;
				slew-rate = <1>;
		};
		pins2 {
				pinmux = <STM32_PINMUX('A', 2, AF11)>; /* ETH1_MDIO */
				bias-disable;
				drive-push-pull;
				slew-rate = <0>;
		};
		pins3 {
				pinmux = <STM32_PINMUX('A', 7, AF11)>, /* ETH1_CRS_DV */
						 <STM32_PINMUX('C', 4, AF11)>, /* ETH1_RXD0 */
						 <STM32_PINMUX('C', 5, AF11)>, /* ETH1_RXD1 */
						 <STM32_PINMUX('G', 12, AF11)>; /* ETH1_PHY_INTN */
				bias-disable;
		};
		pins4 {
				pinmux = <STM32_PINMUX('B', 11, AF11)>; /* ETH1_TX_EN */
		};
};

And the ethernet values:

&ethernet0 {
 status = "okay";
 pinctrl-0 = <&ethernet0_rmii_pins>;
 pinctrl-names = "default";
 phy-mode = "rmii";
 phy-handle = <&phy0>;
 max-speed = <100>;
 
 mdio0 {
 #address-cells = <1>;
 #size-cells = <0>;
 compatible = "snps,dwmac-mdio";
 phy0: ethernet-phy@0 {
 compatible = "ethernet-phy-ieee802.3-c22";
 reg = <0>;
 };
 };
};

I'm using the default stm32mp157.dtsi:

ethernet0: ethernet@5800a000 {
		compatible = "st,stm32mp1-dwmac", "snps,dwmac-4.20a";
		reg = <0x5800a000 0x2000>;
		reg-names = "stmmaceth";
		interrupts-extended = <&intc GIC_SPI 61 IRQ_TYPE_LEVEL_HIGH>,
							 <&intc GIC_SPI 62 IRQ_TYPE_LEVEL_HIGH>,
							 <&exti 70 1>;
		interrupt-names = "macirq",
						 "eth_wake_irq",
						 "stm32_pwr_wakeup";
		clock-names = "stmmaceth",
					 "mac-clk-tx",
					 "mac-clk-rx",
					 "ethstp";
		clocks = <&rcc ETHMAC>,
				 <&rcc ETHTX>,
				 <&rcc ETHRX>,
				 <&rcc ETHSTP>;
		st,syscon = <&syscfg 0x4>;
		snps,mixed-burst;
		snps,pbl = <2>;
		snps,en-tx-lpi-clockgating;
		snps,axi-config = <&stmmac_axi_config_0>;
		snps,tso;
		power-domains = <&pd_core>;
		status = "disabled";
};

Under linux, a generic phy gets detected, and phytool also shows us data, but wrong values:

Configuring network interfaces... [ 6.162488] Generic PHY stmmac-0:00: attached PHY driver [Generic PHY] (mii_bus:phy_addr=stmmac-0:00, irq=POLL)
[ 6.183019] dwmac4: Master AXI performs any burst length
[ 6.187173] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 6.194290] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 6.203155] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[ 6.210029] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 7.276918] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 10Mbps/Half - flow control off
[ 7.283904] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
 
....
root@bytedevkit:~# phytool print eth0/0
ieee-phy: id:0x0000ffff
 
 ieee-phy: reg:BMCR(0x00) val:0000
 flags: -reset -loopback -aneg-enable -power-down -isolate -aneg-restart -collision-test
 speed: 10-half
 
 ieee-phy: reg:BMSR(0x01) val:0xffff
 capabilities: +100-b4 +100-f +100-h +10-f +10-h +100-t2-f +100-t2-h
 flags: +ext-status +aneg-complete +remote-fault +aneg-capable +link +jabber +ext-register

The phy id is wrong: 0x0000ffff and should be 0x20005ca0.

Reading any register outputs 0x0000 and 0xfffff alternating.

The TI DP83848CVV driver is built in into the kernel:

root@bytedevkit:~# zcat /proc/config.gz | grep 8384
CONFIG_DP83848_PHY=y

 I appreciate any help here, thank you.

This topic has been closed for replies.

3 replies

PatrickF
ST Employee
July 22, 2020

Hello,

I'm more on the HW side, so I will cover only those aspects.

I understand you are in this situation: https://wiki.st.com/stm32mpu/wiki/Ethernet_device_tree_configuration#RMII_with_Crystal_on_PHY_-28Reference_clock_-28standard_RMII_clock_name-29_is_provided_by_a_Phy_Crystal-29

Maybe an MDIO bus issue (address, or HW related such as pull-up, voltage, frequency).

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
KKett.1
KKett.1Author
Associate
July 22, 2020

Hello Patrick,

yes, "3.3.1 RMII with Crystal on PHY (Reference clock (standard RMII clock name) is provided by a Phy Crystal)" is our situation.

I'm checking tomorrow with our HW engineer and will report back.

What do you mean with mdio address? The reg = <0> value in phy0?

Thank you.

Best regards,

Kevin

KKett.1
KKett.1Author
Associate
July 24, 2020

The PHY now works.

There were two issues:

  1. Missing reset on the PHY reset line (phy just didn't respond)
  2. Wrong phy address

Our pinctrl definitions are now these:

ethernet0_rmii_pins: rmii-0 {
		pins1 {
				pinmux = <STM32_PINMUX('A', 1, AF11)>, /* ETH1_REF_CLK */
						 <STM32_PINMUX('B', 12, AF11)>, /* ETH1_TXD0 */
						 <STM32_PINMUX('C', 1, AF11)>, /* ETH1_MDC */
						 <STM32_PINMUX('G', 14, AF11)>; /* ETH1_TXD1 */
				bias-disable;
				drive-push-pull;
				slew-rate = <1>;
		};
		pins2 {
				pinmux = <STM32_PINMUX('A', 2, AF11)>; /* ETH1_MDIO */
				bias-pull-up;
				drive-push-pull;
				slew-rate = <0>;
		};
		pins3 {
				pinmux = <STM32_PINMUX('A', 7, AF11)>, /* ETH1_CRS_DV */
						 <STM32_PINMUX('C', 4, AF11)>, /* ETH1_RXD0 */
						 <STM32_PINMUX('C', 5, AF11)>, /* ETH1_RXD1 */
						 <STM32_PINMUX('G', 12, AF11)>; /* ETH1_PHY_INTN */
				bias-disable;
		};
		pins4 {
				pinmux = <STM32_PINMUX('B', 11, AF11)>; /* ETH1_TX_EN */
		};
};

And our ethernet definition:

&ethernet0 {
 status = "okay";
 pinctrl-0 = <&ethernet0_rmii_pins>;
 pinctrl-names = "default";
 phy-mode = "rmii";
 phy-handle = <&phy0>;
 max-speed = <100>;
		
 snps,reset-delays-us = <0>, <10000>, <1000000>;
 snps,reset-gpio = <&gpiob 5 GPIO_ACTIVE_LOW>;
 snps,reset-active-low = <1>;
 
 mdio0 {
 #address-cells = <1>;
 #size-cells = <0>;
 compatible = "snps,dwmac-mdio";
 
 phy0: ethernet-phy@1 {
 reg = <0x01>;
 };
 };
};