Skip to main content
Associate II
May 13, 2025 9:17 AM UTC
Solved

Trouble reading differential ADC channel on STM32MP157C under Linux

I am trying to measure voltages using the STM32MP157C's built-in ADC on channel 18 in differential mode, but keep getting wrong values. Linux kernel is 6.1.28.

Here are the relevant bits from the Linux device tree:

&pinctrl {
    adc_pins_mx: adc_mx-0 {
        pins {
            pinmux = <STM32_PINMUX('A', 4, ANALOG)>, /* ADC1_INP18 */
                     <STM32_PINMUX('A', 5, ANALOG)>; /* ADC1_INN18 */
        };
    };
};

&adc1 {
    status = "okay";
    assigned-resolution-bits = <16>;

    channel@18 {
        reg = <18>;
        diff-channels = <18 18>;
        st,min-sample-time-ns = <10000>;
    };
};


Voltmeter readings:

  • 1.71 mV between INP18 (PA4) and GND
  • 1.39 mV between INN18 (PA5) and GND
  • 0.32 mV between INP18 and INN18

IIO values in /sys/bus/iio/devices/iio:device0:

  • in_voltage-voltage_offset = -32768
  • in_voltage-voltage_scale = 0.100708007
  • in_voltage18-voltage18_raw = 37273

So that's (37273 + -32768) * 0.100708007 = ~453.69 mV instead of the expected 0.32 mV as per Voltmeter.

In single-ended mode ("diff-channels" property removed), the IIO values make more sense:

  • in_voltage_offset = 0
  • in_voltage_scale = 0.050354003
  • in_voltage18_raw = 22

Here I get (22 + 0) * 0.050354003 = ~1.11 mV, which is close enough to the 1.71 mV measured by the voltmeter.

In differential mode, it looks like the computed values are off by a factor of 1000. I am, however, unsure if the "diff-channels" value is correct.

Am I doing this wrong? Is there a bug in the ADC driver in kernel 6.1?

Thanks and best regards,
Robert

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
May 13, 2025 12:49 PM UTC

Hi @rtie ,

as per Reference Manual and Datasheet, differential inputs are supposed to be bias at VREF+/2 +/-10%

PatrickF_0-1747140411772.png

PatrickF_1-1747140515483.png

 

This could explain the bad conversion results.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

2 replies

PatrickF
PatrickFBest answer
ST Employee
May 13, 2025 12:49 PM UTC

Hi @rtie ,

as per Reference Manual and Datasheet, differential inputs are supposed to be bias at VREF+/2 +/-10%

PatrickF_0-1747140411772.png

PatrickF_1-1747140515483.png

 

This could explain the bad conversion results.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
rtieAuthor
Associate II
May 16, 2025 8:27 AM UTC

Ah, I see. Our input signals are not centered around 1.65 V, so they are completely out of range. We'll change our hardware accordingly.

Thank you very much!