Skip to main content
ALeba.1
Associate
August 23, 2024
Solved

Trouble Flashing STM32DDRFW-UTIL over USB

Background:

I'm trying to bring up a custom board with an STM32MP157D and DDR3. When I tried flashing the BSP, I got an error: "ERROR: DDR addr bus test: can't access memory @ 0xc0000004". I decided to try using STM32DDRFW-UTIL to test the DDR before proceeding. I downloaded the code and compiled and debugged the project for an STM32MP157C-DK2. The image sucessfully loaded via the ST-Link in engineering mode and I saw the UART with the expected DDR tool interface. My custom board does not have an ST-Link connection, so I was going to try to flash the image into sysram using USB. I'm still working with the DK2 as a proof of concept.

Issue:

When I try to flash the image using STM32_Programmer_CLI, the utility does not start. I am using the binary in the Binaries folder of STM32DDRFW-UTIL and trying to flash it with "STM32_Programmer_CLI -c port=usb1 -d STM32MP157C-DK2_DDR_UTILITIES_A7.stm32 0x01 -s 0x01". I get the following output and nothing on the UART:

-------------------------------------------------------------------
STM32CubeProgrammer v2.17.0
-------------------------------------------------------------------




USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 002000203338510634383330
DFU protocol: 1.1
Board : --
Device ID : 0x0500
Device name : STM32MP15xx
Device type : MPU
Revision ID : --
Device CPU : Cortex-A7


Memory Programming ...
Opening and parsing file: STM32MP157C-DK2_DDR_UTILITIES_A7.stm32
File : STM32MP157C-DK2_DDR_UTILITIES_A7.stm32
Size : 61.22 KB
Partition ID : 0x01

Download in Progress:
[==================================================] 100%

File download complete
Time elapsed during download operation: 00:00:00.461

RUNNING Program ...
Address: : 0x1
Error:
Unable to reconnect the target device: time out expired
Error: Start operation failed

 How can I get this working? For reference, I'm running this on Linux.

 

Thanks for any help!

This topic has been closed for replies.
ALeba.1
ALeba.1Best answer
Associate
August 26, 2024

I've figured it out!

It looks like something that was previously fixed, but a commit two months ago wiped out the fix:

Here's the change that got wiped out from Scripts/imageheader/postbuild_STM32MP15.sh:

ALeba1_0-1724679805753.png

By adding this change back in, the file loads into SYSRAM successfully.

1 reply

ALeba.1
ALeba.1AuthorBest answer
Associate
August 26, 2024

I've figured it out!

It looks like something that was previously fixed, but a commit two months ago wiped out the fix:

Here's the change that got wiped out from Scripts/imageheader/postbuild_STM32MP15.sh:

ALeba1_0-1724679805753.png

By adding this change back in, the file loads into SYSRAM successfully.