Skip to main content
Associate
May 29, 2025 5:12 AM UTC
Question

To add a partition in tsv file by edit yocto receipe

Hi STM:

I'm developing with developer package and want to add a slot like below 

PED 0x12 rootfs2 ENV mmc1 0x44A00000 none

or

PED 0x12 rootfs2 ENV mmc1 0x44A00000 st-image-core-openstlinux-weston-stm32mp13-disco.root2fs.ext4

 

About the second case

I have modified layers/meta-st/meta-st-stm32mp/conf/machine/include/st-machine-flashlayout-stm32mp.inc, add below 

STM32MP_ROOTFS2_LABEL ?= "rootfs2"
STM32MP_ROOTFS2_SIZE ?= "1048576"
STM32MP_ROOTFS2_IMAGE ?= "st-image-root2fs"

PARTITIONS_IMAGES[rootfs2] = "${STM32MP_ROOTFS2_IMAGE},${STM32MP_ROOTFS2_LABEL},,${STM32MP_ROOTFS2_SIZE},FileSystem"

STM32MP_ROOTFS2_PROGRAMMER_NAME ?= "rootfs2"
FLASHLAYOUT_PARTITION_ENABLE:${STM32MP_ROOTFS2_PROGRAMMER_NAME} = "PED"
FLASHLAYOUT_PARTITION_ID:${STM32MP_ROOTFS2_PROGRAMMER_NAME} = "0x15"

STM32MP_ROOTFS2_MOUNTPOINT ?= "/usr/rootfs2"
ST_ROOTFS2 ?= "1"
PARTITIONS_CONFIG[rootfs2] = "${STM32MP_ROOTFS2_IMAGE},${STM32MP_ROOTFS2_LABEL},${STM32MP_ROOTFS2_MOUNTPOINT},${STM32MP_ROOTFS2_SIZE},FileSystem"


PARTITIONS_LIST += "rootfs2"
PARTITIONS_LIST_EFI += "rootfs2"

 

But the tsv file is not generated with below warning

Cannot generate FlashLayout_emmc_stm32mp135f-dk-optee.tsv file: the st-image-root2fs-openstlinux-weston-stm32mp13-disco.rootfs2.ext4 binary for rootfs2 partition is missing in deploy folder

 

Please kindly help to provide any suggest

Many thanks

 

This topic has been closed for replies.

3 replies

Associate
May 29, 2025 5:50 AM UTC

Hi STM:

Update:

I am trying to generate the rootfs2 image and add below 

cat layers/meta-st/meta-st-stm32mp/recipes-st/images/st-image-rootfs2.bb

SUMMARY = "STM32MP rootfs2 Image"
LICENSE = "MIT"

include recipes-st/images/st-image-partitions.inc

IMAGE_NAME_SUFFIX = ".rootfs2"

# Define to null ROOTFS_MAXSIZE
IMAGE_ROOTFS_MAXSIZE = ""

# Add specific package for our image:
PACKAGE_INSTALL += " \
"

But get below error
WARNING: st-image-rootfs2-1.0-r0 do_image: Not able to locate /etc/build file in image rootfs /build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs
ERROR: st-image-rootfs2-1.0-r0 do_image: ExecutionError('/build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/temp/run.reformat_rootfs.1177898', 1, None, None)
ERROR: Logfile of failure stored in: /build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/temp/log.do_image.1177898
Log data follows:
| DEBUG: Executing python function do_image
| NOTE: Executing extract_buildinfo ...
| DEBUG: Executing python function extract_buildinfo
| WARNING: Not able to locate /etc/build file in image rootfs /build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs
| DEBUG: Python function extract_buildinfo finished
| NOTE: Executing systemd_preset_all ...
| DEBUG: Executing shell function systemd_preset_all
| DEBUG: Shell function systemd_preset_all finished
| NOTE: Executing reproducible_final_image_task ...
| DEBUG: Executing shell function reproducible_final_image_task
| NOTE: reproducible_final_image_task: mtime set to 1723296920
| DEBUG: Shell function reproducible_final_image_task finished
| NOTE: Executing reformat_rootfs ...
| DEBUG: Executing shell function reformat_rootfs
| NOTE: Mountpoint found in /build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs
| NOTE: >>> Remove all files and folder except
| NOTE: >>> Move contents to /build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs
| mv: '/build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs/bin' and '/build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs/bin' are the same file
| mv: '/build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs/etc' and '/build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs/etc' are the same file
| mv: '/build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs/lib' and '/build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs/lib' are the same file
| mv: '/build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs/sbin' and '/build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs/sbin' are the same file
| mv: '/build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs/usr' and '/build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs/usr' are the same file
| mv: '/build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs/var' and '/build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/build-openstlinuxweston-stm32mp13-disco/tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/st-image-rootfs2/1.0/rootfs/var' are the same file
| WARNING: exit code 1 from a shell command.
| DEBUG: Python function do_image finished
ERROR: Task (/build/jordan/workspace/STM/mp131c_vry/shst2-re1/project_build/layers/meta-st/meta-st-stm32mp/recipes-st/images/st-image-rootfs2.bb:do_image) failed with exit code '1'
NOTE: Tasks Summary: Attempted 6492 tasks of which 6483 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 2 seconds

Thank you

Christophe Guibout
ST Technical Moderator
Jun 3, 2025 11:59 AM UTC

Hello @Jordan_Lin,

 

This mechanism to build TSV files is usefull for ST to manage SoC/board diversity, but if you use only one TSV file, I would recommand to use an hardcoded TSV file.

In your manchine, you can add the following lines to point to your TSV file which will be deployed after:

ENABLE_FLASHLAYOUT_DEFAULT = "1"

FLASHLAYOUT_DEFAULT_SRC = " \

files/flashlayouts/optee/myFlashLayout1.tsv \

files/flashlayouts/optee/myFlashLayout2.tsv \"

   

BR,

Christophe

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
Jun 5, 2025 2:10 AM UTC

Hi Christophe::

Thanks for reply

Would you provide me some advices that which recipe file is proper for me  to add the lines?

Maybe like below bb file?

layers/meta-st/meta-st-openstlinux/recipes-core/systemd/systemd-mount-partitions.bb

 

And i create a new directory like 

layers/meta-st/meta-st-openstlinux/recipes-core/systemd/files/flashlayouts/optee/

and put the hardcoded tsv file below it

Then if the modification is work, the tsv file will occur in below directory?

build-openstlinuxweston-stm32mp13-disco/tmp-glibc/deploy/images/stm32mp13-disco/flashlayout_st-image-core/optee/

 

Thank you for help

Jordan