Hi,
sound normal that your don't find it in your custom project.
Location and presence of this definition depend on how the project DT has been sourced:
- In Upstreamed Started Package DT, it is located in stm32mp157a-dk1-u-boot.dtsi file. See https://wiki.st.com/stm32mpu/wiki/STM32MP15_device_tree#U-Boot
- In CubeMx generated DT for board STM32MP157A-DK1, you should find it in stm32mp157a-YOURCUBEMXPROJECT-mx-u-boot.dtsi file. See https://wiki.st.com/stm32mpu/wiki/STM32MP15_device_tree#U-Boot_2
- In CubeMx generated DT for a custom board project, this definition will not be present (as it is linked to DK1 or DK2 board hardware)
- So, by default, there is neither no u-Boot warnings nor worries related to USB-C CC lines.
- It should be added manually if needed (which is not your case as you don't plan to have USB-C as in DK1/DK2)
Regards.
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent