Skip to main content
Ffu.1
Associate II
November 25, 2021
Solved

The problem with facilitating uboot errors

  • November 25, 2021
  • 4 replies
  • 2566 views

When compiling the U-boot, these four commands are used:

PC $& gt; export KBUILD_OUTPUT=.. /build/stm32mp15_trusted

PC $& gt; export DEVICE_TREE=stm32mp157c-dk2

PC $& gt; make stm32mp15_trusted_defconfig

PC $& gt; make all

use the first: export KBUILD_OUTPUT=.. /build/stm32mp15_trusted, the compiler will fail, but if there is no first statement, the compiler will succeed

This topic has been closed for replies.
Best answer by Kevin HUBER

Hello @Ffu.1​ ,

The error displayed about "make mrproper", means that your build folder is not clean and was already used with another configuration or with another build directory.

So please, run this command to clean your directory

make mrproper

Then redo the commands:

export KBUILD_OUTPUT=../build/stm32mp15_trusted
make stm32mp15_trusted_defconfig

And specify the device tree in the make all command :

make DEVICE_TREE=stm32mp157c-dk2 all

Regards,

Kevin

4 replies

Kevin HUBER
Kevin HUBERBest answer
ST Employee
November 25, 2021

Hello @Ffu.1​ ,

The error displayed about "make mrproper", means that your build folder is not clean and was already used with another configuration or with another build directory.

So please, run this command to clean your directory

make mrproper

Then redo the commands:

export KBUILD_OUTPUT=../build/stm32mp15_trusted
make stm32mp15_trusted_defconfig

And specify the device tree in the make all command :

make DEVICE_TREE=stm32mp157c-dk2 all

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Ffu.1
Ffu.1Author
Associate II
November 26, 2021

This does work, but why only u-boot.bin is generated, not u-boot.stm32

Kevin HUBER
ST Employee
November 26, 2021

Hi @Ffu.1​ ,

Yes, I assume that you are using an ecosystem v3.0.0 or 3.1.0. It is normal that you do not have a u-boot.stm32.

Since the ecosystem v3.0.0, two binaries are needed from u-boot:

https://wiki.st.com/stm32mpu/wiki/U-Boot_overview#Output_files

u-boot.dtb and u-boot-nodtb.bin

The .stm32 is now a tf-a.stm32. To learn more things about the FIP, you can read the ecosystem release note: https://wiki.st.com/stm32mpu/wiki/STM32MP15_ecosystem_release_note_-_v3.0.0#OpenSTLinux_-28Cortex-C2-AE-A7-29

or this part of the TF-A overview: https://wiki.st.com/stm32mpu/wiki/TF-A_overview#FIP

The FIP can be generated automatically when you build your TF-A, please have a look to the README.HOW_TO.txt of the TF-A.

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Kevin HUBER
ST Employee
December 1, 2021

Hello @Ffu.1​ ,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.