Skip to main content
milkylainen
Associate III
August 8, 2022
Question

TF-A v2.6-r1 kernel hang issue?

I have a custom build on the stm32mp157f dk2.

stm TF-A v2.6-r1 or vanilla TF-A v2.7, using sp_min.

stm U-boot 2020.10-r2 or vanilla Barebox-2022.06.

I've also tried U-boot 2021.10-r1, but that one crashes the kernel even earlier.

Kernel: vanilla 5.18/vanilla 5.19.

FSBL starts fine.

Both v2.6 and v2.7 starts just fine. sp_min too.

Both TF-A versions load and executes BL33 (stm u-boot or vanilla barebox) just fine.

But when I use stm TF-A v2.6 kernel crashes when started from BL33.

Works fine with vanilla TF-A 2.7 all other components being equal.

I can see the kernel decompression but stops executing directly after that.

This happens regardless if I do the fip manually or if TF-A puts it together.

Kernel 5.18 or 5.19 doesn't matter. But when I use vanilla TF-A both kernels boot.

TF-A is configured exactly the same using the variable configuration.

This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
September 1, 2022

Hi @milkylainen​ ,

Sorry to come late in the thread.

First do you still have issue or did you manage to fix it by yourself ?

Thanks,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
milkylainen
Associate III
September 1, 2022

Hi Olivier.

Np. I am still having this issue.

I have a hard time mixing parts of the ecosystem with vanilla.

So the only configuration I have gotten to a working userland is

vanilla tf-a 2.7, stm u-boot 2020.10, vanilla kernel 5.18+.

If I go to stm tf-a 2.6-r1, kernel crashes.