Skip to main content
Associate
December 28, 2023
Solved

TF-A hangs on stm32mp157d-dk1

Hello all, 

As part of the evaluation of the 32MP15 series, I was trying to build the u-boot and TF-A binaries. 
I tried the u-boot SPL bring up and it seems to be working fine (except for failure to launch the Linux Kernel, as per your late updates). 

For U-boot, I used : https://github.com/STMicroelectronics/u-boot

And Build commands:
   $  make -j12 stm32mp15_defconfig
   $  make -j12 DEVICE_TREE=stm32mp157d-dk1 all


For TF-A binary, I used : https://github.com/STMicroelectronics/arm-trusted-firmware/tree/v2.8-stm32mp
And Build command of BL32 (SP MIN mode):
$ make -j12 ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 AARCH32_SP=sp_min DTB_FILE_NAME=stm32mp157d-dk1.dtb bl32 dtbs

and Build command of BL2: 
make -j12 ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_SDMMC=1 STM32MP15=1 DTB_FILE_NAME=stm32mp157d-dk1.dtb LOG_LEVEL=40 DEBUG=1

 

and to generate FIP binary from TF-A Makefile, I used: 
$ make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 AARCH32_SP=sp_min DTB_FILE_NAME=stm32mp157d-dk1.dtb BL33=../u-boot/build_custom_stmp32mp15/u-boot-nodtb.bin BL33_CFG=../u-boot/build_custom_stmp32mp15/u-boot.dtb fip

Using the fip.bin & tf-a-stm32mp157d-dk1.stm32 , 
The TF-A failed to load the kernel and kept resetting, the following log was showed up: 

NOTICE: CPU: STM32MP157DAC Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157D-DK1 Discovery Board
NOTICE: Board: MB1272 Var3.0 Rev.C-02
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: PMIC version = 0x21
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.4-r2.3(debug):v2.4-stm32mp-r2.3
NOTICE: BL2: Built : 23:18:08, Dec 28 2023
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2: Loading image id 31
INFO: Loading image id=31 at address 0x2ffff000
INFO: Image id=31 loaded: 0x2ffff000 - 0x2ffff226
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffc5000
INFO: Image id=4 loaded: 0x2ffc5000 - 0x2ffd6590
WARNING: Not a known TEE, use default loading options.
INFO: BL2: Skip loading image id 21
INFO: BL2: Skip loading image id 22
INFO: BL2: Loading image id 23
INFO: Loading image id=23 at address 0xc0500000
INFO: Image id=23 loaded: 0xc0500000 - 0xc051ee40
INFO: BL2: Loading image id 26
INFO: Loading image id=26 at address 0x2ffc0000
INFO: Image id=26 loaded: 0x2ffc0000 - 0x2ffc477d
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: Image id=5 loaded: 0xc0100000 - 0xc01f1d6c
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffc5000
INFO: SPSR = 0x1d3
NOTICE: SP_MIN: v2.4-r2.3(release):v2.4-stm32mp-r2.3
NOTICE: SP_MIN: Built : 23:17:24, Dec 28 2023
NOTICE: CPU: STM32MP157DAC Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157D-DK1 Discovery Board
NOTICE: Board: MB1272 Var3.0 Rev.C-02
INFO: Reset reason (0x54):
INFO: System reset generated by MPU (MPSYSRST)
INFO: PMIC version = 0x21

Note that if I replace the fip and TF-A with the ones generated by Yocto build, the Linux Kernel boots up. 
So what could be causing TF-A to reboot right after boot BL32? 

This topic has been closed for replies.
Erwan SZYMANSKI
Erwan SZYMANSKIBest answer
ST Technical Moderator
January 2, 2024

Hello @MuhammadTharwat ,
On which OpenSTLinux are you working on ? Could you consider to use OP-TEE instead of sp_min ? SP_MIN is no more supported on our recent deliveries.

Kind regards,
Erwan. 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

7 replies

Erwan SZYMANSKI
Erwan SZYMANSKIBest answer
ST Technical Moderator
January 2, 2024

Hello @MuhammadTharwat ,
On which OpenSTLinux are you working on ? Could you consider to use OP-TEE instead of sp_min ? SP_MIN is no more supported on our recent deliveries.

Kind regards,
Erwan. 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
January 2, 2024

Hello Erwan, 

The problem is not OpenSTLinux , I can confirm that it is the problem of U-boot. 
I was using v2022.10-stm32mp & v2021.10-stm32mp and that did have the problem. When I switched to v2020.10-stm32mp, it works as expected. 
So could that be attributed to the deprecated use of SP Min ?

BR, 
Muhammad

Erwan SZYMANSKI
ST Technical Moderator
January 2, 2024

@MuhammadTharwat ,
Great to hear that you tackled your issue. Hard to confirm for SP_MIN as I do not have enough information to do it. What is sure is that components version delivered in one OpenSTLinux release should be kept aligned to work properly.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
January 2, 2024

I'm using openstlinux-5.10. 
That still uses U-boot v2020.10-stm32mp-r2.2 in SP Min mode (as per the commit history and U-boot start-up logs)

so the U-boot versions  v2022.10-stm32mp & v2021.10-stm32mp  are broken ???