Skip to main content
ASkri.1
Senior
May 27, 2021
Question

tf-a and u-boot custom compile fails

Hi, Everybody!

Referring to this issue:

https://community.st.com/s/question/0D53W00000oVNtqSAG/qaudspi-spinand-flash-device-tree-for-tfa-and-uboot

PatrickF suggested to manually configure U-BOOT for my board. I have downloaded tf-a sources patched it, of course installed and configured SDK and trying to do all according to it's README.HOW_TO.txt file.

As I have my specific DT I need to specify it in makefile parameters:

README.HOW_TO.txt has this example:

make -f $PWD/../Makefile.sdk TFA_DEVICETREE=stm32mp157c-ev1 TF_A_CONFIG=trusted ELF_DEBUG_ENABLE='1' all

But in fact TFA_DEVICETREE var-name should be TF_A_DEVICETREE. Is this correct?

Then, file format. We have .stm32, also .fip file format avaialble

I can compile both .stm32 tf-a and u-boot, but u-boot fail to start with following error:

NOTICE: CPU: STM32MP157DAB Rev.Z

NOTICE: Model: STMicroelectronics STM32MP157A-DK1 STM32CubeMX board

INFO:  Reset reason (0x14):

INFO:   Pad Reset from NRST

INFO:  PMIC version = 0x21

INFO:  FCONF: Reading TB_FW firmware configuration file from: 0x2ffe3000

INFO:  FCONF: Reading firmware configuration information for: stm32mp_io

INFO:  Using USB

INFO:   Instance 2

INFO:  Boot used partition fsbl1

NOTICE: BL2: v2.4-r1.0(debug):

NOTICE: BL2: Built : 11:12:52, May 27 2021

INFO:  BL2: Doing platform setup

INFO:  RAM: DDR3-DDR3L 16bits 533000Khz

WARNING: Couldn't find property st,phy-cal in dtb

INFO:  Memory size = 0x20000000 (512 MB)

INFO:  DFU USB START...

INFO:  phase ID :0, Manifestation 0 at c00001d9

INFO:  phase ID :3, Manifestation 3 at c80e1fa2

ERROR:  FIP Header check failed for phase 3

ERROR:  usb_core_ctl_error : Send an ERROR

INFO:  handle USB : Suspend int

INFO:  USB Suspend mode

Then I'm trying to compile tf-a with fip option, but it fails with following error:

 make -f ../Makefile.sdk TF_A_CONFIG=trusted TF_A_DEVICETREE=stm32mp157a-stm32mp151-dk1-mx fip

fiptool-stm32mp config:

 optee:

  bl32 config value: optee

 trusted:

  bl32 config value: tfa

 FIP_DEVICETREE: stm32mp157a-stm32mp151-dk1-mx

 FIP_DEPLOYDIR_FIP  : /home/screep/Distribution-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/FIP_artifacts//fip

 FIP_DEPLOYDIR_TFA  : /home/screep/Distribution-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-2.4.r1-r0/tf-a-sources/../deploy/bl32

 FIP_DEPLOYDIR_FWCONF: /home/screep/Distribution-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-2.4.r1-r0/tf-a-sources/../deploy/fwconfig

 FIP_DEPLOYDIR_OPTEE : /home/screep/Distribution-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/FIP_artifacts//optee

 FIP_DEPLOYDIR_UBOOT : /home/screep/Distribution-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/FIP_artifacts//u-boot

Missing stm32mp157a-stm32mp151-dk1-mx-fw-config-optee.dtb file in folder: $FIP_DEPLOYDIR_FWCONF or '$FIP_DEPLOYDIR_ROOT/arm-trusted-firmware/fwconfig'

Why optee? I don;t need optee.

Can anybody help me with correct sequence compiling tf-a and u-boot starting from source download and finishing with success kernel load...

Thank you in advance

Looking forward for your reply

This topic has been closed for replies.

20 replies

PatrickF
ST Employee
May 28, 2021
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
ASkri.1
ASkri.1Author
Senior
May 31, 2021
Hi, Patrick!
Thank you very much for your reply. Finally I've got tf-a and u-boot assembled and FIP image generated.
(using this wiki page: https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package#U-boot_-_unpack_and_patch_sources
)
But u-boot load fails with following log:
NOTICE: CPU: STM32MP157DAB Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157A-DK1 STM32CubeMX board
INFO: Reset reason (0x14):
INFO: Pad Reset from NRST
INFO: PMIC version = 0x21
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe3000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.4-r1.0(debug):
NOTICE: BL2: Built : 13:48:10, May 31 2021
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
WARNING: Couldn't find property st,phy-cal in dtb
INFO: Memory size = 0x20000000 (512 MB)
INFO: DFU USB START...
INFO: phase ID :0, Manifestation 0 at c0000141
INFO: phase ID :3, Manifestation 3 at c80feba4
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 31
INFO: Loading image id=31 at address 0x2ffff000
WARNING: Image id=31 size out of bounds
ERROR: BL2: Failed to load image id 31 (-27)
Here is flash-layout file:
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl-boot Binary none 0x0
./tf-a-stm32mp157a-stm32mp151-dk1-mx-usb.stm32
- 0x03 fip-boot Binary none 0x0
./fip-stm32mp157a-stm32mp151-dk1-mx-trusted.bin
#P 0x04 fsbl1 Binary mmc0 boot1
../../arm-trusted-firmware/tf-a-stm32mp157a-stm32mp151-dk1-mx-trusted.stm32
#P 0x05 fsbl2 Binary mmc0 boot2
../../arm-trusted-firmware/tf-a-stm32mp157a-stm32mp151-dk1-mx-trusted.stm32
#P 0x06 ssbl Binary mmc0 0x00080000
../../bootloader/u-boot-stm32mp157a-stm32mp151-dk1-mx-trusted.stm32
#P 0x21 boot System mmc0 0x00280000
../../st-image-bootfs-openstlinux-weston-stm32mp1-disco-mx.ext4
#P 0x22 vendorfs FileSystem mmc0 0x04280000
../../st-image-vendorfs-openstlinux-weston-stm32mp1-disco-mx.ext4
#P 0x23 rootfs FileSystem mmc0 0x05280000
../../st-image-weston-openstlinux-weston-stm32mp1-disco-mx.ext4
#P 0x24 userfs FileSystem mmc0 0x33C80000
../../st-image-userfs-openstlinux-weston-stm32mp1-disco-mx.ext4
Here is CubeMXProgrammer output:
PatrickF
ST Employee
May 31, 2021

Hi,

Btw, your fail is within TF-A.

I suspect something not well formed in the uBoot FIP image around FW_CONFIG size.

On Flashing DK2, I see :

INFO:   Loading image id=31 at address 0x2ffff000

INFO:   Image id=31 loaded: 0x2ffff000 - 0x2ffff226

INFO:   FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000

INFO:   FCONF: Reading firmware configuration information for: dyn_cfg

INFO:   FCONF: Reading firmware configuration information for: stm32mp1_firewall

Note that device column = mmc0 mean SD-Card on SDMMC.

To build a Serial-NAND CubeProgrammer Flashlayout, please have a look to https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#NAND_Flash_memory_with_FIP

Device column should be spi-nand0 and offset to be carefully selected (see also https://wiki.st.com/stm32mpu/wiki/STM32MP15_Flash_mapping#NAND_memory_mapping)

Regards

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent