Skip to main content
Oitsh.1
Associate
May 19, 2020
Question

Tamper pins

Is there any application note for tamper pins? Which one of the pins is the active tamper?

This topic has been closed for replies.

2 replies

PatrickF
ST Employee
May 19, 2020

Hello,

Active Tamper need a couple of pins, TAMP_OUT and TAMP_IN, connected on PCB by various security mechanism (wires, mesh, switch, sensors, etc..).

Examples of connections are:

  • TAMP_OUT3 on PC13 connected to TAMP_IN3 on PC1

or

  • TAMP_OUT2 on PC13 connected to TAMP_IN2 on PI8

or

  • TAMP_OUT2 (or TAMP_OUT3) on PC13 connected to TAMP_IN2 on PI8 and TAMP_IN3 on PC1 (two tampers input on same output)

or

  • TAMP_OUT3 on PI8 connected to TAMP_IN1 on PC13 and TAMP_IN3 on PC1 (two tampers input on same output)

Regards

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Oitsh.1
Oitsh.1Author
Associate
August 9, 2020

Hi Patrick,

I'm using the 257 pins package of the STM32MP153 with Ethernet.

So PC1 is used for ETH_MDC.

PI8 is not available because of the package.

Does this means I can't use active tamper?

Regards,

Ofer