Skip to main content
SYEH
Associate II
Nov 22, 2019 6:41 AM UTC
Solved

STPMIC1 - PONKEYn POWER_ON POWER_DOWN trigger

For STPMIC1, when it is powered on by asserting the PONKEYn signal low, what would happen if the PONKEYn remains asserted low even after the initial POWER_ON trigger? Would it subsequently trigger a POWER_DOWN if PONKEYn long press turn off is activated? Or is the PONKEYn event triggered only when there is a HIGH to LOW edge transition (edge trigger) ?

Thanks.

Steven

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Nov 26, 2019 1:36 PM UTC

Hi @SYEH​ 

In that case STPMIC1 will not trig a POWER DOWN. You need another HIGH to LOW edge transition to start the Long Key Press timer.

Hope it help,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

4 replies

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Nov 26, 2019 1:36 PM UTC

Hi @SYEH​ 

In that case STPMIC1 will not trig a POWER DOWN. You need another HIGH to LOW edge transition to start the Long Key Press timer.

Hope it help,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SYEH
SYEHAuthor
Associate II
Nov 26, 2019 2:17 PM UTC

Hi Olivier,

Thanks for the reply. Understood.

Is that the same for the WAKEUP pin? As in the WAKEUP POWER_ON event will only trigger from LOW to HIGH edge transition, and does not require to stay HIGH after the initial trigger?

Thanks.

Steven.

Olivier GALLIEN
ST Technical Moderator
Nov 26, 2019 2:44 PM UTC

Yes WAKEUP pin is edge sensitive. Except in the situation explain in DataSheet Figure 58. Turn-on condition before VIN_POR_Rise.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.