Skip to main content
Lead
Feb 18, 2025 2:16 PM UTC
Solved

STM32N6 vs STM32MP257 - Which one have the best AI?

I have seen a lot of videos on YouTube where STM32N6 demonstrates incredible AI features such as multiple pose estimation, multiple object detection and multiple object classification at the same time.

But I haven't seen anything similar for STM32MP257. So my question is: If I want to start with AI on embedded systems, which one of them two should I use? 

This topic has been closed for replies.
GatienC
GatienCBest answer
ST Employee
Feb 20, 2025 9:03 AM UTC

Hello @DMårt,

Please find this small presentation video describing the AI capabilities on stm32mp257 platforms :

STM32MP25 NPU - AI tools 

 

There, you have a description of the embedded NPU on stm32mp257: STM32MP25 NPU wiki (up to 1.35TOPS)

Application examples: https://wiki.st.com/stm32mpu/wiki/Category:AI_-_Application_examples 

X-Linux-AI expansion package: https://wiki.st.com/stm32mpu/wiki/Category:X-LINUX-AI_expansion_package 

 

Best regards,

Gatien

5 replies

mbarg.1
Senior III
Feb 18, 2025 2:32 PM UTC

Well, N6 is built with AI in mind and has dedicated resources for that !

DMårtAuthor
Lead
Feb 18, 2025 2:47 PM UTC

@mbarg.1 

Can you elaborate that?

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
mbarg.1
Senior III
Feb 18, 2025 3:20 PM UTC

From STM web site STM32N6 series - STMicroelectronics :

The STM32N6 is the first STM32 MCU to embed the ST Neural-ART accelerator™, an in-house developed neural processing unit (NPU) engineered for power-efficient edge AI applications. Clocked at 1 GHz and providing up to 600 GOPS, it enables real-time neural network inference for computer vision and audio applications.

A dedicated computer vision pipeline with a MIPI CSI-2 interface and image signal processing (ISP) ensures compatibility with a wide range of cameras. The STM32N6 also features an H264 hardware encoder and the NeoChrom™ Accelerator for graphics, making it suitable for feature-rich products.

It offers 4.2 Mbytes of contiguous embedded RAM, ideal for neural networks or graphics applications, complemented by high-speed external memory interfaces (hexa-SPI, OCTOSPI, FMC).

DMårtAuthor
Lead
Feb 20, 2025 7:43 AM UTC

Can anyone from ST show me some demonstrations for the STM32MP257 when AI is used?

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
GatienC
GatienCBest answer
ST Employee
Feb 20, 2025 9:03 AM UTC

Hello @DMårt,

Please find this small presentation video describing the AI capabilities on stm32mp257 platforms :

STM32MP25 NPU - AI tools 

 

There, you have a description of the embedded NPU on stm32mp257: STM32MP25 NPU wiki (up to 1.35TOPS)

Application examples: https://wiki.st.com/stm32mpu/wiki/Category:AI_-_Application_examples 

X-Linux-AI expansion package: https://wiki.st.com/stm32mpu/wiki/Category:X-LINUX-AI_expansion_package 

 

Best regards,

Gatien