Skip to main content
ARehm
Associate II
August 5, 2022
Solved

STM32mpu157c-dk2 Distribution package failed to 96% while doing do_rootfs

st-image-resize-initrd-1.0-r0 do_rootfs: Unable to update the package index files

st-image-vendorfs-1.0-r0 do_rootfs: Unable to update the package index files

Anyone know how to fix this.

Already have applied clean build.

Build Configuration:

BB_VERSION          = "2.0.0"

BUILD_SYS           = "x86_64-linux"

NATIVELSBSTRING     = "universal"

TARGET_SYS          = "arm-ostl-linux-gnueabi"

MACHINE             = "stm32mp15-disco"

DISTRO              = "openstlinux-weston"

DISTRO_VERSION      = "4.0.1-snapshot-20220805"

TUNE_FEATURES       = "arm vfp cortexa7 neon vfpv4 thumb callconvention-hard"

TARGET_FPU          = "hard"

DISTRO_CODENAME     = "kirkstone"

ACCEPT_EULA_stm32mp15-disco = "1"

GCCVERSION          = "11.%"

PREFERRED_PROVIDER_virtual/kernel = "linux-stm32mp"

meta-python         

meta-oe             

meta-gnome          

meta-initramfs      

meta-multimedia     

meta-networking     

meta-webserver      

meta-filesystems    

meta-perl           = "HEAD:0b78362654262145415df8211052442823b9ec9b"

meta-st-stm32mp     = "HEAD:d00d3a076e103c549c5d7dbcd587269c863e97cb"

meta-qt5            = "HEAD:5b71df60e523423b9df6793de9387f87a149ac42"

meta-st-openstlinux = "HEAD:182b150c45ef874fb3bebc3ac5ba0ed784790938"

meta                = "HEAD:cb8647c08959abb1d6b7c2b3a34b4b415f66d7ee"

 Errors:

Command '['/home/ARehm/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Distribution-Package/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/stm32mp15_disco-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/recipe-sysroot-native/usr/bin/apt-get', 'update']' returned 100:

Thanks

This topic has been closed for replies.
ARehm
ARehmBest answer
Associate II
August 6, 2022

I have solved this problem. The problem was long path which is describe in the tutorial. Make sure keep short path for example :

mkdir $HOME/st_dist

cd $HOME/st_dist

//again create short name dir such as

mkdir openstlinux

cd openstlinux

// now install repo manually if not install in you PC by using below command

mkdir -p ~/.bin

PATH="${HOME}/.bin:${PATH}"

curl https://storage.googleapis.com/git-repo-downloads/repo > ~/.bin/repo

chmod a+rx ~/.bin/repo

//now run

repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15

repo sync

//Now you need to run ;

DISTRO=openstlinux-weston MACHINE="stm32mp15-disco" source layers/meta-st/scripts/envsetup.sh build

//here "build" is the directory name at the end of the command if you don not give //the name it will take //default name which is again long name no need for that

bitbake st-image-weston

@FOR ST:

please make sure you default paths should not excced the OS requirement.

4 replies

ARehm
ARehmAuthor
Associate II
August 5, 2022

Here is my log file

ARehm
ARehmAuthor
Associate II
August 5, 2022

Here is the log file

ARehm
ARehmAuthorBest answer
Associate II
August 6, 2022

I have solved this problem. The problem was long path which is describe in the tutorial. Make sure keep short path for example :

mkdir $HOME/st_dist

cd $HOME/st_dist

//again create short name dir such as

mkdir openstlinux

cd openstlinux

// now install repo manually if not install in you PC by using below command

mkdir -p ~/.bin

PATH="${HOME}/.bin:${PATH}"

curl https://storage.googleapis.com/git-repo-downloads/repo > ~/.bin/repo

chmod a+rx ~/.bin/repo

//now run

repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15

repo sync

//Now you need to run ;

DISTRO=openstlinux-weston MACHINE="stm32mp15-disco" source layers/meta-st/scripts/envsetup.sh build

//here "build" is the directory name at the end of the command if you don not give //the name it will take //default name which is again long name no need for that

bitbake st-image-weston

@FOR ST:

please make sure you default paths should not excced the OS requirement.

超汪.1
Visitor II
August 19, 2022

I had the same problem