Skip to main content
Associate II
Apr 29, 2025 5:06 AM UTC
Solved

STM32MP257F-DK wifi bt

Hi there,

I'm using STM32MP257F-DK and bringing up by FlashLayout_emmc_stm32mp257f-dk-ca35tdcid-ostl-optee.tsv.
I found there is no wifi/bt device by command ifconfig. It's only showing below.

 

root@stm32mp2:/etc# ifconfig
end0 Link encap:Ethernet HWaddr 10:E7:7A:E3:AA:F4
inet6 addr: fe80::12e7:7aff:fee3:aaf4/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:102 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:28558 (27.8 KiB)
Interrupt:58

lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:130 errors:0 dropped:0 overruns:0 frame:0
TX packets:130 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:9985 (9.7 KiB) TX bytes:9985 (9.7 KiB)

usb0 Link encap:Ethernet HWaddr DA:74:68:4A:DE:B0
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

 

May I confirm how to enable wifi/bt?

 

Thank you!
Mason

This topic has been closed for replies.
Erwan SZYMANSKI
Erwan SZYMANSKIBest answer
ST Technical Moderator
Apr 29, 2025 6:48 AM UTC

Hello @MasonPan0804 ,
You have a wiki article providing the guidelines here: https://wiki.st.com/stm32mpu/index.php?title=How_to_setup_a_WLAN_connection&sfr=stm32mpu

Please can you try to follow it ?

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

3 replies

Erwan SZYMANSKI
Erwan SZYMANSKIBest answer
ST Technical Moderator
Apr 29, 2025 6:48 AM UTC

Hello @MasonPan0804 ,
You have a wiki article providing the guidelines here: https://wiki.st.com/stm32mpu/index.php?title=How_to_setup_a_WLAN_connection&sfr=stm32mpu

Please can you try to follow it ?

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
Apr 29, 2025 7:15 AM UTC

Hi,

There is no wlan0 after emmc boot, how to do the next?

Thank you!

Mason

Associate II
Apr 29, 2025 7:17 AM UTC

sorry, i found the wlan0 using ifconfig -a, thank you!