Lead
Mar 21, 2025 8:56 AM UTC
Solved
STM32MP257F-DK LVDS connector questions
- 2 replies
- 1148 views
This question is a based on of a support ticket due to more knowledge persons from ST may answer this on the forum. Hope someone can help.
- Any specific reason to use this type of LVDS connector instead of 40pin FPC ? (less costly connector and cable, easier for development)
- Do you have recommended LVDS cable to ST's LVDS LCD ? I-PEX 81422-100B-02-D ? or what does ST use for testing/development ?
- Any recommendation for any LVDS to FPC 0.5mm pitch conversion cable ?
- What is the part-number of the LVDS receptable on the board. Is it I-PEX 20455-040E or another brand ?
- Is it the same connector on LCD side ? if not, what connector is used at the LCD side ?
- What is the suggestion for the LVDS plug on the cable ? I-PEX 20453 ?
- It seems there isn't a standard for LVDS cable pinout, correct ? Is there any standard or reference ST used for the pin assignment ?