Skip to main content
Ronte.1
Associate III
Jun 18, 2025 7:56 AM UTC
Solved

STM32MP257F-DK GStreamer problem

Hello,

I'm using Buildroot environment with the STM32MP257F-DK board. I'm testing GStreamer with a simple pipeline:

gst-launch-1.0 videotestsrc ! autovideosink

When I first run it there is no problem. The test video shows fine on the HDMI monitor. But when I run it again second time there are errors : pipeline doesn't want to preroll. And all attempts after that fail too. It works only one time after the boot.

There is additional debug info: drmModeSetPlane failed: No space left on device (28).

Maybe some setting is missing ?

BR

raimo

This topic has been closed for replies.
PPAGE.13
PPAGE.13Best answer
ST Employee
Jun 27, 2025 7:16 AM UTC

Hi Raimo,

if you are fine with your last gstreamer parameters, please close the ticket.

Have a good day.

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

6 replies

PPAGE.13
ST Employee
Jun 18, 2025 10:02 AM UTC

Hi,

 

in OSTL Yocto based environment, there is no issue running several times your gstreamer command.

 

In you Builtroot env, you can try to check CMA  memory with this command into a shell script:

"while true ; do grep CmaFree /proc/meminfo ; sleep 3 ; done"

 

And also try a bigger and HW accelerated mp4 video with the similar command to that:

su -l weston -c "gst-launch-1.0 filesrc location=/usr/local/demo/medical/videos/air_1024.mp4 ! qtdemux ! h264parse ! queue ! v4l2slh264dec ! autovideosink"

 

(replace mp4 file with yours)

 

Note: to check HW VPU is activated, check interrrupts number:

"cat /proc/interrupts | grep vdec"

 

BR,

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Ronte.1
Ronte.1Author
Associate III
Jun 18, 2025 10:31 AM UTC

Hi,

I did the CMA check, first it shows CmaFree 129400kB

After a succesful gstreamer launch there was 120976 kB, and after next failing tries there's 128800 kB and it doesnt change after this.  

BR Raimo

 

 

PPAGE.13
ST Employee
Jun 18, 2025 11:58 AM UTC

Hi,

 

could you please add "-v" option in you gstreamer command to get more info.

 

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Ronte.1
Ronte.1Author
Associate III
Jun 18, 2025 1:01 PM UTC

Hi,

Here's the log file when launch fails:

 

# gst-launch-1.0 videotestsrc ! autovideosink -v
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
/GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0/GstKMSSink:autovideosink0-actual-sink-kms: display-width = 1920
/GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0/GstKMSSink:autovideosink0-actual-sink-kms: display-height = 1080
/GstPipeline:pipeline0/GstVideoTestSrc:videotestsrc0.GstPad:src: caps = video/x-raw, format=(string)BGRA, width=(int)320, height=(int)240, framerate=(fraction)30/1, multiview-mode=(string)mono, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive
/GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0.GstGhostPad:sink.GstProxyPad:proxypad0: caps = video/x-raw, format=(string)BGRA, width=(int)320, height=(int)240, framerate=(fraction)30/1, multiview-mode=(string)mono, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive
/GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0/GstKMSSink:autovideosink0-actual-sink-kms.GstPad:sink: caps = video/x-raw, format=(string)BGRA, width=(int)320, height=(int)240, framerate=(fraction)30/1, multiview-mode=(string)mono, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive
/GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0.GstGhostPad:sink: caps = video/x-raw, format=(string)BGRA, width=(int)320, height=(int)240, framerate=(fraction)30/1, multiview-mode=(string)mono, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive
ERROR: from element /GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0/GstKMSSink:autovideosink0-actual-sink-kms: GStreamer encountered a general resource error.
Additional debug info:
../sys/kms/gstkmssink.c(2032): gst_kms_sink_show_frame (): /GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0/GstKMSSink:autovideosink0-actual-sink-kms:
drmModeSetPlane failed: No space left on device (28)
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
ERROR: from element /GstPipeline:pipeline0/GstVideoTestSrc:videotestsrc0: Internal data stream error.
Additional debug info:
../libs/gst/base/gstbasesrc.c(3132): gst_base_src_loop (): /GstPipeline:pipeline0/GstVideoTestSrc:videotestsrc0:
streaming stopped, reason error (-5)
ERROR: pipeline doesn't want to preroll.
Freeing pipeline ...
#

 

BR Raimo

Ronte.1
Ronte.1Author
Associate III
Jun 23, 2025 7:45 AM UTC

Hi,

I found a sort of cure for this.

If I add some parameters to the sink then the launch will work all times.

gst-launch-1.0 videotestsrc ! kmssink driver-name=stm connector-id=32 force-modesetting=true.

In my setup the kmssink was the one the autovideosink is choosing.

BR Raimo

 

PPAGE.13
PPAGE.13Best answer
ST Employee
Jun 27, 2025 7:16 AM UTC

Hi Raimo,

if you are fine with your last gstreamer parameters, please close the ticket.

Have a good day.

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.