Skip to main content
Associate II
May 7, 2025 9:10 AM UTC
Question

STM32MP257F-DK CM33 peripheral initialization crashes A35

I generated the M33 code using CubeIDE by following the lab manual.

During the driver initializations:
MX_ADC1_Init();
MX_I2C1_Init();
MX_ICACHE_Init();
MX_RTC_Init();

The A35 halts CPU1 and resets after sometime.

E/TC:0 stm32_iac_itr:192 IAC exceptions [159:128]: 0x10000000
E/TC:0 stm32_iac_itr:197 IAC exception ID: 156
E/TC:0 Panic at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r1/core/drivers/firewall/stm32_iac.c:212 <stm32_iac_itr>
E/TC:0 TEE load address @ 0x82000000
E/TC:0 Call stack:
E/TC:0 0x82007ed8
E/TC:0 0x82041b44
E/TC:0 0x8202c2c0
E/TC:0 0x8203f678
E/TC:0 0x82013cf4
E/TC:0 0x820017dc
I/TC: Halting CPU 1

Unfortunately I failed to create astable functional M33 for my MPU project yet. Are there no proper manual of code generation and configuration?

This topic has been closed for replies.

7 replies

Associate II
May 7, 2025 9:17 AM UTC

Attached is the ioc file.

Olivier GALLIEN
ST Technical Moderator
May 7, 2025 9:30 AM UTC

Hi @partha_sarathi1000 ,

You are facing issue related to RIFF configuration. 

If you generate project using CubeMX you might carefully consider the RIFF configuration pane. ( RIFSC for peripheral assignement, RISAB and RISAF for memory ) 

Refer the related documentation on Wiki and in RM : 

https://wiki.st.com/stm32mpu/wiki/RIFSC_internal_peripheral

https://wiki.st.com/stm32mpu/wiki/RISAB_internal_peripheral

https://wiki.st.com/stm32mpu/wiki/RISAF_internal_peripheral

Olivier 

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
May 7, 2025 1:03 PM UTC

Thanks @Olivier GALLIEN for the reply.

But did config RIF as per manual.

What I have found that its crashing during GPIO RCC enable macros, like:
__HAL_RCC_GPIOI_CLK_ENABLE();

So in any peripheral initialization, wherever there is any GPIO RCC clock enable statement in its respective _MspInit() function, I commented them out and then the initialization passed without any issue.

I tested UART is working with that. But I don't think its a solution.

Regards
Partha

Visitor II
Jun 29, 2025 9:40 PM UTC

Hello,

I am facing the exact same problem with this board when creating a blank project in STM32CubeIDE.

The provided examples of the STM32MP2 package work, but they don't have any ioc CubeMX configuration file that would allow me to make my own project.

Would it be possible to make the blank project work ?

Visitor II
Jun 29, 2025 9:42 PM UTC

@Olivier GALLIENI can report the same problem on my end with this board, I can't get a blank M33 project to work. Would you have any tip ?

PatrickF
ST Employee
Jun 30, 2025 12:13 PM UTC

Hi,

Not RIF expert, but according to 


IAC exception ID: 156

this is referring to an illegal access to the RCC (i.e. CM33 might not have write access to the RCC register used for instance to enable a clock). So your findings are in right direction. Probably the GPIOI should be defined as shared in RCC (GPIOI is RCC resource 98)

Unfortunately, I cannot help you to set the right config in CubeMx.

Regards.

 

 

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
ST Employee
Jul 2, 2025 10:16 PM UTC

Hi @partha_sarathi1000 ,

To work on the M33, use the template provided in the firmware package. This template is compatible with the Starter Package.

I believe your issue arises because you are building M33 firmware with an RIF configuration that differs from the one used by the A35. Are you using the Starter Package image?

Which board are you using?

Best regards,
Febus