Skip to main content
Visitor II
Aug 13, 2025 7:55 AM UTC
Question

STM32MP257 programming via JTAG

Hello, we are currently designing a STM32MP257 based custom board. For reference, we are looking into STM32MP257F-EV1 and STM32MP257-DK evaluation kit schematics. In both schematics, there is an STM32 MCU which connects to the JTAG ports of the STM32MP257. Is this MCU used as an STLINK to provide JTAG to USB2.0 conversion? If so, if we are to implement the same structure on our board, is there a way to access the STLINK firmware and embed it into our own MCU? Furthermore, is there an external STLINK adapter dedicated for STM32MP25 series MPUs to access JTAG over USB?

My second question is that can we program the MPU using the JTAG pins? Both in reference manual and datasheet of the MPU, there doesn't seem to be a boot mode setting for JTAG.

 

This topic has been closed for replies.

1 reply

Olivier GALLIEN
ST Technical Moderator
Sep 25, 2025 7:24 AM UTC

Hi @mert_ozgur 

 

STLINK-V3MODS | Tool - STMicroelectronics looks to be what you need to integrate STLINK in a custom board

Else external probe is also available. 

 

MP257 can't be programmed by JTAG but only through DFU USB/Serial.  JTAG/STLink can be used anyway to debug with STM32CubeIDE

 

Have a look to wiki to get useful guidance stm32mpu 

 

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.