Skip to main content
Associate III
Sep 28, 2025 3:50 AM UTC
Solved

stm32mp2 RT patches ,CPUFreq can't use

Due to the default removal of CPUFreq configuration in the patch file after applying RTpatch, I am unable to obtain the current CPU frequency through the following command.

reference:如何更改 CPU 频率 - stm32mpu

I also try lscpu and /proc/cpuinfo and so on.

They can't solve it. I checked the CPU frequency

Is there any other way?

 

This topic has been closed for replies.
Christophe Guibout
ST Technical Moderator
Oct 9, 2025 11:33 AM UTC

Hello @bugman,

 

The default CPU clock is 1.2GHz with X-LINUX-RT : the frequency is fixed following the recommended industrial profile (wiki link).

You can change the frequency, but the SoC won't follow the recommended industrial profile anymore.

 

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

4 replies

Christophe Guibout
ST Technical Moderator
Oct 3, 2025 12:47 PM UTC

Hello @bugman,

 

As cpufreq is disabled in X-LINUX-RT, I would recommand to check the CPU frequency through clock summary:

cat /sys/kernel/debug/clk/clk_summary | grep ck_cpu1

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
bugmanAuthor
Associate III
Oct 9, 2025 10:13 AM UTC

bugman_0-1760004403986.png

I am using The CPU model: STM32MP257DAL ,Displayed as 1.2Ghz through the command line you provided.

According to the instructions on the wiki, the clock speed can reach 1.5GHz. Is the default speed 1.2GHz used in the RT version ? 

Can the frequency be changed to 1.2GHz?

Christophe Guibout
ST Technical Moderator
Oct 9, 2025 11:33 AM UTC

Hello @bugman,

 

The default CPU clock is 1.2GHz with X-LINUX-RT : the frequency is fixed following the recommended industrial profile (wiki link).

You can change the frequency, but the SoC won't follow the recommended industrial profile anymore.

 

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.