Skip to main content
Lead
Jun 7, 2025 11:19 PM UTC
Solved

STM32MP2 does not have USB OTG - SD card is the only option then?

At STM32MP1, there is an USB OTG, were you can flash the eMMC via the USB OTG. 

But in STM32MP2, there is no USB OTG. Does this mean that I need to flash my SD-card instead? Just like Raspberry Pi etc.?

Or am I supposed to flash the eMMC via the USB C connector?

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
Jun 9, 2025 10:02 AM UTC

HI @DMårt 

in STM32MP2, USB3DR IP is the equivalent of OTG seen on STM32MP1.

You flashload using USB type-C or USB micro-B in same way.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

1 reply

PatrickF
PatrickFBest answer
ST Employee
Jun 9, 2025 10:02 AM UTC

HI @DMårt 

in STM32MP2, USB3DR IP is the equivalent of OTG seen on STM32MP1.

You flashload using USB type-C or USB micro-B in same way.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent